hi,
use IMX8 EVK board, set PMIC power output,after kernel is start。
but PMIC ->PMIC_I2C,
DTB no PIMC_i2c config ,i donot know how to do?
Hi WANG
pmic usage with i.mx8 series is described in Linux Manual
from Linux 4.19.35_1.1.0 Documentation
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
How does the kernel communicate with SCFW? Using the API: sc_pm_get_sys_power_mode,
Are there any examples of using apis in the kernel?
To modify the SCFW code, can only change the PMIC voltage output before kernel startup.
I think APP can also call API to modify the PMIC voltage output when running linux APP after kernel startup。
>How does the kernel communicate with SCFW?
example (SC_R_MU_1A) :