IMX7D LCDIFx_AS_CTRL field descriptions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX7D LCDIFx_AS_CTRL field descriptions

675件の閲覧回数
864535720
Contributor II

Hello everyone
In the IMX7DRM manual, there is a description of the LCDIFx_AS_CTRL register on page 4286. In the description of bits 19-16 of the LCDIFx_AS_CTRL register, there is some understanding of the description.
MASKAS = 0x0 AS AND PS
MASKNOTAS = 0x1 nAS AND PS
MASKASNOT = 0x2 AS AND nPS
MERGEAS = 0x3 AS OR PS
MERGENOTAS = 0x4 nAS OR PS
MERGEASNOT = 0x5 AS OR nPS
NOTCOPYAS = 0x6 nAS
NOT = 0x7 nPS
NOTMASKAS = 0x8 AS NAND PS
NOTMERGEAS = 0x9 AS NOR PS
XORAS = 0xA AS XOR PS
NOTXORAS = 0xB AS XNOR PS
In the above description: What is AS? What is PS? What is nAS? What is nPS?
What will be the effect of AS, PS, AND, nAS, OR, XNOR?

ラベル(3)
0 件の賞賛
返信
1 返信

612件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 其东 刘 

>What is AS?,What is PS?

AS is Alpha Surface, PS is single processed surface as described on page 4603.

"nAS" seems inverted AS.

some alpha examples  can be found in

pxp_v4l2_test.c\pxp_v4l2_test\test - imx-test - i.MX Driver Test Application Software 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信