IMX7 SABRESD latest BSP and update details?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX7 SABRESD latest BSP and update details?

Jump to solution
1,786 Views
gopinathsriniva
Contributor III

Hello Everyone,

We are doing custom board based on IMX7 sabresd. I have just started to port BSP for IMX7. When checking for yocto source for IMX7, I have downloaded the "fsl_yocto-L4.1.15_2.0.0-ga.tar.gz" document from the below link.

i.MX 7Dual Arm Cortex-A7 Processor|NXP  

I have followed "i.MX Yocto Project User's Guide" for yocto buil for IMX7. I just want to confirm below are the latest official sources for roots, kernel and u-boot as of today. 

Rootfs                 -  Release L4.1.15_2.0.0_ga for Yocto Project 2.1 (Krogoth).

kernel repo         -  git://git.freescale.com/imx/linux-imx.git;  Branch : remotes/origin/imx_4.1.15_2.0.0_ga

u-boot repo        -   git://git.freescale.com/imx/uboot-imx.git; Branch : remotes/origin/imx_v2016.03_4.1.15_2.0.0_ga

Can you please confirm the same? Also when can we expect the next official update for yocoto/kernel/u-boot for IMX7 BSP and what will be the updates frequency?

Cheers,

Gopinath S 

Labels (2)
0 Kudos
Reply
1 Solution
896 Views
Yuri
NXP Employee
NXP Employee

Hello,

   generally You are right - the recommended release for i.MX7 is L4.1.15.2.0. 

You may try the demo image :

http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0_iMX7D&appType=license&location=null&Parent_... 

Nevertheless, the recent BSP, also supporting i.MX7, is L4.1.15.2.1.

http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.1.0_LINUX_DOCS&Parent_nodeId=133769948107170617... 

Summary page :

i.MX 6 / i.MX 7 Series Software and Development Tool|NXP 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
897 Views
Yuri
NXP Employee
NXP Employee

Hello,

   generally You are right - the recommended release for i.MX7 is L4.1.15.2.0. 

You may try the demo image :

http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0_iMX7D&appType=license&location=null&Parent_... 

Nevertheless, the recent BSP, also supporting i.MX7, is L4.1.15.2.1.

http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.1.0_LINUX_DOCS&Parent_nodeId=133769948107170617... 

Summary page :

i.MX 6 / i.MX 7 Series Software and Development Tool|NXP 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply