IMX6SLL boot config

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,976件の閲覧回数
vlintilhac
Contributor III

Hi,

 

I'm on a custom board with a IMX6SLL chip.

I'm debugging using a JTAG link and would like to change the boot configuration through the JTAG port.

I want to use the SD card as the boot device, but I don't have access to the LCD_GPIOs used to override the BOOT_CFG signals. 

Can I use the JTAG to change the booting configuration and set the SD card as the boot device? What registers should I modified to achieve it? And what address should I point to reboot the chip using the new config?

 

Best,

Vincent

 

Vincent 

0 件の賞賛
返信
1 解決策
1,968件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vincent

 

in general boot configuration is latched at POR in SRC_SBMR1, SRC_SBMR2 registers

(read only),described in sect.41.7.2 SRC Boot Mode Register 1 (SRC_SBMR1)

i.MX 6SLL Applications Processor Reference Manual

so seems it is not possible to use jtag for changing the booting configuration.

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,969件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vincent

 

in general boot configuration is latched at POR in SRC_SBMR1, SRC_SBMR2 registers

(read only),described in sect.41.7.2 SRC Boot Mode Register 1 (SRC_SBMR1)

i.MX 6SLL Applications Processor Reference Manual

so seems it is not possible to use jtag for changing the booting configuration.

 

Best regards
igor

0 件の賞賛
返信