Hi,
This could be a longshot. I received this tablet. It has android 4.0 ICS on it. My question is, how could I find out the u-boot parameters on it? I would like to put the JB4.3_1.1.0 GA release on it. Building would not be a problem as I have already done that, but when it is flashed it will not come on. This is an actual tablet. Is there a way to get the information needed to get it to come on? According to the build prop it looks like a sabresd rom on a sabrelite board. I have tried to find where to hook it up usb to ttl, but it is not marked. I think the key is in the u-boot, but again it would be how to open the image. The basics are the same:
Kernel Base Address : 0x10800000
Ramdisk Load Address : 0x11800000
Second Stage Load Address : 0x11700000
Page Size : 2048 bytes
Is there some software for this? It would be nice to see this build on actual tablet in the real world. Anything would help.
Thanks,
已解决! 转到解答。
Hi Dave
actually I see there both:
"ro.product.name=sabresd_6dq
ro.product.device=sabresd_6dq
ro.product.board=SABRELITE"
You can start with
IMX6_R13.41_ANDROID_DEMO_IMAGE : i.MX 6Quad, i.MX 6Dual, and i.MX 6DualLite Android 13.4.1 BSP Binary Demo Files.
Tool for flashing (through USB)
IMX_6DQ_MFG_TOOL : Tool and documentation for downloading OS images to the i.MX 6Quad and i.MX6Dual.
On the page below one can find Linux and more new Android images
i.MX6Q: i.MX 6Quad Family of Applications Processors
For Uboot "printenv" one needs immediately to hit keyboard when Uboot
just starting, then it enters to command mode (without hitting he jumps loading Android).
Best regards
chip
Hi,
For anyone interested, I have a new question to do with this tablet here: IMX6Q Tablet Problem 2
I really could use some help. Thanks.
Hi Dave
I think first you should identify thing you are using.
Sabre Lite board is supported by Boundary Devices
http://boundarydevices.com/android-on-i-mx6-sabre-lite-and-nitrogen6x/
Freescale boards are Sabre SDP/SDB/AI they are quite different and supported by
Freescale, you can start with link below
i.MX6Q: i.MX 6Quad Family of Applications Processors
Also many other third parties produce own i.MX6 boards.
Uboot parameters can be found with printenv command
http://www.denx.de/wiki/publish/DULG/to-delete/UBootCmdGroupEnvironment.html
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Chip,
Here is what I have found out:
root@android:/ # cat /proc/cpuinfo
Processor : ARMv7 Processor rev 10 (v7l)
processor : 0
BogoMIPS : 790.52
processor : 1
BogoMIPS : 790.52
Features : swp half thumb fastmult vfp edsp neon vfpv3
CPU implementer : 0x41
CPU architecture: 7
CPU variant : 0x2
CPU part : 0xc09
CPU revision : 10
Hardware : Freescale i.MX 6Quad/DualLite/Solo Sabre-SD Board
Revision : 63012
Serial : 0000000000000000
The build prop shows:
# begin build properties
# autogenerated by buildinfo.sh
ro.build.id=R13.4-beta
ro.build.display.id=R13.4-beta
ro.build.version.incremental=eng.android.20121012.113904
ro.build.version.sdk=15
ro.build.version.codename=REL
ro.build.version.release=4.0.4
ro.build.date=Fri Oct 12 11:39:35 CST 2012
ro.build.date.utc=1350013175
ro.build.type=user
ro.build.user=android
ro.build.host=amdroid
ro.build.tags=test-keys
ro.product.model=ICS AOSP on imx6q
ro.product.brand=freescale
ro.product.name=sabresd_6dq
ro.product.device=sabresd_6dq
ro.product.board=SABRELITE
ro.product.cpu.abi=armeabi-v7a
ro.product.cpu.abi2=armeabi
ro.product.manufacturer=unknown
ro.product.locale.language=en
ro.product.locale.region=US
ro.wifi.channels=
ro.board.platform=imx6
# ro.build.product is obsolete; use ro.product.device
ro.build.product=sabresd_6dq
# Do not try to parse ro.build.description or .fingerprint
ro.build.description=sabresd_6dq-user 4.0.4 R13.4-beta eng.android.20121012.113904 test-keys
ro.build.fingerprint=freescale/sabresd_6dq/sabresd_6dq:4.0.4/R13.4-beta/eng.android.20121012.113904:user/test-keys
ro.build.characteristics=default
# end build properties
# system.prop for M1 reference board
# This overrides settings in the products/generic/system.prop file
#
hw.hasethernet=true
#
# ADDITIONAL_BUILD_PROPERTIES
#
ro.config.notification_sound=OnTheHunt.ogg
ro.config.alarm_alert=Alarm_Classic.ogg
hw.hasethernet=true
dalvik.vm.heapstartsize=20m
dalvik.vm.heapgrowthlimit=200m
dalvik.vm.heapsize=320m
net.bt.name=Android
dalvik.vm.stack-trace-file=/data/anr/traces.txt
Which board would it be; SABERLITE or sabresd? My guess would now be the sabresd in light of the cpuinfo. I ave never used the printenv command. Do I use it in an adb shell or do I just get in the directory with u-boot.bin and type:
$ printenv u-boot.bin
Thank you for help,
Dave
Hi Dave
actually I see there both:
"ro.product.name=sabresd_6dq
ro.product.device=sabresd_6dq
ro.product.board=SABRELITE"
You can start with
IMX6_R13.41_ANDROID_DEMO_IMAGE : i.MX 6Quad, i.MX 6Dual, and i.MX 6DualLite Android 13.4.1 BSP Binary Demo Files.
Tool for flashing (through USB)
IMX_6DQ_MFG_TOOL : Tool and documentation for downloading OS images to the i.MX 6Quad and i.MX6Dual.
On the page below one can find Linux and more new Android images
i.MX6Q: i.MX 6Quad Family of Applications Processors
For Uboot "printenv" one needs immediately to hit keyboard when Uboot
just starting, then it enters to command mode (without hitting he jumps loading Android).
Best regards
chip
Hi Chip,
I have not been able to get the "printenv" command to work. I there any possible way to open the u-boot.bin? I mean if it is built, then it could be un-built, so to speak. After all, it is a type of data file. This is what I do know:
base@there:~/myroms$ file uImage_update
uImage_update: u-boot legacy uImage, Linux-3.0.35, Linux/ARM, OS Kernel Image (Not compressed), 6470076 bytes, Mon Nov 19 03:58:55 2012, Load Address: 0x10008000, Entry Point: 0x10008000, Header CRC: 0x9DD6CF62, Data CRC: 0xCC806858
and this:
base@there:~/myroms$ binwalk uImage_update
DECIMAL HEX DESCRIPTION
-------------------------------------------------------------------------------------------------------
0 0x0 uImage header, header size: 64 bytes, header CRC: 0x9DD6CF62, created: Mon Nov 19 03:58:55 2012, image size: 6470076 bytes, Data Address: 0x10008000, Entry Point: 0x10008000, data CRC: 0xCC806858, OS: Linux, CPU: ARM, image type: OS Kernel Image, compression type: none, image name: "Linux-3.0.35"
18340 0x47A4 gzip compressed data, from Unix, NULL date: Wed Dec 31 17:00:00 1969, max compression
As you can see they called it uImage_update instead of u-boot.bin. It looks like it still does the same thing. This is the only piece of the puzzle to be solved; as it looks like the rest of the rom would be exactly the same (mount points and addresses).
What do you think?
Hi Dave
when board power-up, uboot starts to execute,
immediately in this moment pressing key should stop it and
uboot should enter to command line.
If there is SD slot one can build images below and try them with new SD card
IMX6_JB43_110_ANDROID_SOURCE_BSP :
Best regards
chip
Hi Chip,
Would this be what you are talking about? Is this what I should see?
root@android:/ # printenv
_=/system/bin/printenv
ANDROID_BOOTLOGO=1
ANDROID_PROPERTY_WORKSPACE=8,32768
LOOP_MOUNTPOINT=/mnt/obb
PS1=$(precmd)$USER@$HOSTNAME:${PWD:-?} #
SHM_MOUNTPOINT=/mnt/shm
CODEC_SHM_PATH=/mnt/shm
COMPONENT_REGISTER_FILE=/system/etc/component_register
USER=root
CONTENTPIPE_REGISTER_FILE=/system/etc/contentpipe_register
EXTERNAL_STORAGE=/mnt/sdcard
HOSTNAME=android
ANDROID_DATA=/data
PATH=/sbin:/vendor/bin:/system/sbin:/system/bin:/system/xbin
ASEC_MOUNTPOINT=/mnt/asec
TERM=vt100
MKSH=/system/bin/sh
HOME=/
LD_LIBRARY_PATH=/vendor/lib:/system/lib
SECONDARY_STORAGE=/mnt/extsd:/mnt/udisk
LOGNAME=root
GST_PLUGIN_PATH=/system/lib/gst_plugins
LIGHTSENSOR_PATH=/sys/class/i2c-adapter/i2c-1/1-0044
VPU_FW_PATH=/system/lib/firmware/vpu
CORE_REGISTER_FILE=/system/etc/core_register
BOOTCLASSPATH=/system/framework/core.jar:/system/framework/core-junit.jar:/system/framework/bouncycastle.jar:/system/framework/ext.jar:/system/framework/framework.jar:/system/framework/android.policy.jar:/system/framework/services.jar:/system/framework/apache-xml.jar:/system/framework/filterfw.jar
ANDROID_ROOT=/system
SHELL=/system/bin/sh
ANDROID_ASSETS=/system/app
RANDOM=8203
Thank you,
Hi Dave,
As I mentioned in a message on our blog, I'm confused.
Is this a tablet, or a SABRE Lite?
It's not clear to me whether somebody's buying SABRE Lite boards and putting them in tablets, or if (more likely), they used the SABRE Lite board as a reference and starting point for the kernel and Android and just never bothered to change the names.
In any case, you should ask the vendor to provide the kernel and U-Boot sources. Both are covered under GPL, so it's a copyright violation not to provide those.
Hi Eric,
Yes it is a tablet. I believe they used the SABRE Lite board as a reference. The problem is that I have not been able to get any response whatsoever from the company. I'm hoping that I'm not out of luck on this.
Can you provide details of the make and model of the tablet?
Even if the design was based on SABRE Lite, it's highly likely that the manufacturer made changes, and you'll need to know the details of those before confidently changing U-Boot or the kernel.
Yes, it is a Zenithink (zt-285) C-94. The imx6q version; 10.1". I did manage to pull this off it:
root@android:/ # cat /sys/bus/mmc/devices/mmc0:0001/boot_info
boot_info:0x05;
ALT_BOOT_MODE:1 - Supports alternate boot method
DDR_BOOT_MODE:0 - Does not support dual data rate during boot
HS_BOOTMODE:1 - Supports high speed timing during boot
boot_size:268435456KB
boot_partition:0x00;
BOOT_ACK:0 - No boot acknowledge sent
BOOT_PARTITION-ENABLE: 0 - Device not boot enabled
PARTITION_ACCESS:0 - No access to boot partition
boot_bus:0x00
BOOT_MODE:0 - Use single data rate + backward compatible timings in boot operation
RESET_BOOT_BUS_WIDTH:0 - Reset bus width to x1, single data rate and backwardcompatible timings after boot operation
BOOT_BUS_WIDTH:0 - x1 (sdr) or x4 (ddr) bus width in boot operation mode
There is a boot_config file there and one other boot file, but even with super user rights, I haven't been able to get information from them or even copy. Probably to do with no access to the boot partition. I don't know.
I was hoping to find what may be needed to get this to boot up. I really think it would be something to do with the uImage wrapper, but I am not at all familiar with that nor u-boot. I guess that is beating a dead horse... Is there some way to use u-boot to point at the existing uImage wrapper or uImage? I'm just asking. I thought there was something somewhere I read about that. I really don't know.
The best bet is to try and find the manufacturer, to see if they have some un-bricking tools and also to see if you can get the U-Boot and kernel sources.
Google doesn't seem to help though.
Zenithink seems to be well hidden behind suppliers.
Since they're using an i.MX6, it might make sense to post a separate question to see if anyone knows how to contact them.
He Dave,
if this is Zenithink C94, seems there is no way
to invoke Uboot. It uses customized software with special
update algorithm
[ROM] Zenithink's Official 20121203 ICS ROM - ZT-285 C94 - SlateDroid.com
Best regards
chip