Hi everyone,
I'm using the image fsl-image-gui on the IMX6Q Sabre Board (Poky Yocto project)
For technical reasons, i need to be able to connect an analog camera to the Sabre Board.
Since the sabre board doesn't have any analog video input, i have to use an analog to digital converter.
I found the ADV7282-M which is able to convert CVBS analog video signals into an 8-bit YCrCb 4:2:2 video data stream that is output over a MIPI CSI-2 interface.
I plan on using the ADV7282-M Evaluation board
To me both interfaces on the Sabre board and the ADV7282-M should be compatible and it should work without any problems.
But, to be sure, do you know about any technical or eletrical issues such as voltage and current i/o?
ADV7282-M datasheet:
http://www.analog.com/static/imported-files/data_sheets/ADV7282.pdf
Any pointers would be of great help
Thank you :smileywink:
Solved! Go to Solution.
On SPF-27392 it is J5 (Hirose FX12B-40P-0.4SV), BOM file one can find in
"MX6_SABRE_SDP_DESIGNFILES "
~igor
Hi Philippe
you are right, MIPI CSI-2 is standard interface so
Sabre board and the ADV7282-M should be compatible and work without
problems.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you for your answer.
Is MIPI CSI-2 connected on J9 on the IMX6Q-SDB?
On SPF-27392 it is J5 (Hirose FX12B-40P-0.4SV), BOM file one can find in
"MX6_SABRE_SDP_DESIGNFILES "
~igor
Ok so i need to use the Smart Devices Platform then.
I'll try to find a way to connect the SDP to the evaluation board of the ADV7282M
Thank you very much!
Best regards