IMX6Q Sabre board with ADV7282 compatibily over MIPI interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Q Sabre board with ADV7282 compatibily over MIPI interface

Jump to solution
1,242 Views
philippeballeyd
Contributor IV

Hi everyone,

I'm using the image fsl-image-gui on the IMX6Q Sabre Board (Poky Yocto project)


For technical reasons, i need to be able to connect an analog camera to the Sabre Board.

Since the sabre board doesn't have any analog video input, i have to use an analog to digital converter.

I found the ADV7282-M which is able to convert CVBS analog video signals into an 8-bit YCrCb 4:2:2 video data stream that is output over a MIPI CSI-2 interface.


I plan on using the ADV7282-M Evaluation board


To me both interfaces on the Sabre board and the ADV7282-M should be compatible and it should work without any problems.

But, to be sure, do you know about any technical or eletrical issues such as voltage and current i/o?


ADV7282-M datasheet:

http://www.analog.com/static/imported-files/data_sheets/ADV7282.pdf


Any pointers would be of great help


Thank you :smileywink:

Labels (3)
0 Kudos
1 Solution
676 Views
igorpadykov
NXP Employee
NXP Employee

On SPF-27392 it is J5 (Hirose FX12B-40P-0.4SV), BOM file one can find in

"MX6_SABRE_SDP_DESIGNFILES "

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREPLAT&fpsp=1&tab=Design_Too...

~igor

View solution in original post

0 Kudos
4 Replies
676 Views
igorpadykov
NXP Employee
NXP Employee

Hi Philippe

you are right, MIPI CSI-2 is standard interface so

Sabre board and the ADV7282-M should be compatible and work without

problems.


Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

676 Views
philippeballeyd
Contributor IV

Thank you for your answer.

Is MIPI CSI-2 connected on J9 on the IMX6Q-SDB?

0 Kudos
677 Views
igorpadykov
NXP Employee
NXP Employee

On SPF-27392 it is J5 (Hirose FX12B-40P-0.4SV), BOM file one can find in

"MX6_SABRE_SDP_DESIGNFILES "

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREPLAT&fpsp=1&tab=Design_Too...

~igor

0 Kudos
676 Views
philippeballeyd
Contributor IV

Ok so i need to use the Smart Devices Platform then.

I'll try to find a way to connect the SDP to the evaluation board of the ADV7282M

Thank you very much!

Best regards

0 Kudos