i use IMX6D linux3.10.53
now i want to chang the DDR frequency from 528MHZ to 400MHZ,
First i change 528 to 400 in I.MX6DQSDL DDR3 Script Aid V0.10,and then i use this config to calibration config to do the DDR calibration , and i also have put these configs and it's calibration result to the DCD files in uboot.
Except these, need i to modify other code of kernel or uboot for changing DDR frequency from 528MHZ to 400MHZ?
Thanks.
Hi z
one can port codes for changing ddr frequency to uboot plugin.S
using examples in linux ddr3_freq_imx6.S:
mx6sabresd\freescale\board - uboot-imx - i.MX U-Boot
ddr3_freq_imx6.S\mach-imx\arm\arch - linux-imx - i.MX Linux kernel
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
you shoud change ddr3 frequency running code from OCRAM.