IMX6D 3.14.52 VPU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6D 3.14.52 VPU

2,440 Views
ispsubb
Contributor II

产品在imx6d 3.14.52 这个版本上进行开发。我们在接收 (通过WIFI) iphone  airplay 码流时,imx6在某些场景的码流是不能解码的,表现的现象为卡屏,且不会自动恢复。附件里面有一段在imx6播放的过程中录制的一段H264的码流(附件中的Airplay.264)

这段H264码流在PC上用播放器播放正常。在IMX6 上本地通过以下两种方式播放。

一,gst-launch

gst-launch-1.0  filesrc location=/root/Airplay.264 ! h264parse ! vpudec  ! overlaysink sync=false async=false

视频的后半部分不能解码。

二,mxc_vpu_test.out

./mxc_vpu_test.out -D "-i /root/Airplay.264 -f 2 -a 60

表现异常情况更多。

 

Iphone airplay 中帧率不固定,最高可能到60fps 。在iphone手机横竖屏切换,或者播放iphone手机本地视频时,非常容易出现。@Qiang Li 

Labels (1)
7 Replies

2,142 Views
刘洋
Contributor III

 

I am also studying imx6d, so I can add contact information to facilitate communication. qq: 3054576366

0 Kudos
Reply

2,146 Views
ispsubb
Contributor II

Can yout tell me the command which you had tried ? And your version ?

0 Kudos
Reply

2,146 Views
joanxie
NXP TechSupport
NXP TechSupport

I used "gst-launch-1.0 playbin uri=file:///media/sda1/Airplay.264", /media/sda1/is my path, you can change to yours, the version is 3.10.17,

0 Kudos
Reply

2,146 Views
ispsubb
Contributor II

any one help me ?

0 Kudos
Reply

2,146 Views
joanxie
NXP TechSupport
NXP TechSupport

try to use the playbin, I can play it successfully, any further update, I will follow in the salesfource. you can update your status there. I've reply to you there.

0 Kudos
Reply

2,146 Views
ispsubb
Contributor II

How to play it successfully ?   which BSP ?    3.14.52 ?

0 Kudos
Reply

2,146 Views
joanxie
NXP TechSupport
NXP TechSupport

I used the older version, but you can try the command I mailed to you, any update, you can tell me here or in the saleforce.

0 Kudos
Reply