IMX6 SOLO(MCIMX6S7CVM08AC) I2C Interface Pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 SOLO(MCIMX6S7CVM08AC) I2C Interface Pins

805 Views
emilzachariageo
Contributor II

Hello,

I wanted to interface a MEMS microphone with I2S digital output (Part# ICS‐43434) with my IMXSolo processor.

I wanted IMX to be the master providing the seial data clock and the Frame sync signal.

The audio data from ICS-43434 is to be input by IMX6 RXD pin.

Please comment if the idea and pin connections I've made are correct or not.

pastedImage_2.png

Thanks in advance.

Emil Zacharia George.

Labels (1)
2 Replies

619 Views
igorpadykov
NXP Employee
NXP Employee

Hi Emil

connections look right, for mic usage may be useful to check sect.61.8.4 SSI Clocking,

61.2.1 Signals Overview i.MX6SDL Reference Manual

http://www.nxp.com/assets/documents/data/en/reference-manuals/IMX6SDLRM.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

619 Views
emilzachariageo
Contributor II

Thanks Igor.

0 Kudos
Reply