I have a Freescale IMX6 SabreSD Board with a iMX6 Quad Processor.
Until this morning everything was working fine.
The board was booting Yocto Linux from a SD Card.
I have removed all kernel modules with the command: rmmod *
After reboot the red led is permanently ON.
Did I corrupted the internal flash ?
How to find the flash image to upload via JTAG (if possible) ?
Thank you in advance
Andrea
Solved! Go to Solution.
Hi Andrea, D3 is red while I am at u-boot in my board as well. This should be no problem.
I am not familiar with MFGTool and as mentioned my best suggestion would be to build an uboot
image and place it on SD then boot it from SD. I know this works if your board is fine.
Also, our sabred came with a preloaded SD card that you can boot uboot. If you still have this
original SD you can boot into uboot and you can then boot kernel from there.
Regards
Sinan Akman
Hi Sinan,
the red led is the D3 between the power connector and the SIM card slot.
I don't have a JTAG but I have successfully performed the download of the factory firmware with MFGtool.
Unfortunately the board still cannot boot.
Any suggestion is very welcomed.
Looking forward
Andrea
Hi Andrea, D3 is red while I am at u-boot in my board as well. This should be no problem.
I am not familiar with MFGTool and as mentioned my best suggestion would be to build an uboot
image and place it on SD then boot it from SD. I know this works if your board is fine.
Also, our sabred came with a preloaded SD card that you can boot uboot. If you still have this
original SD you can boot into uboot and you can then boot kernel from there.
Regards
Sinan Akman
Hi Andrea
The SPI is normally not populated on an sabresd board if this
is what you referring to. You can build a u-boot image and
boot your board from SD. If you have a JTAG tool, try to
halt after reset and check if you can read part of ram to make
sure your board is alive. I am not sure which red light you
are referring to. Perhaps you can check in its user guide to
see what a red led is indicating.
In either way, if your board is still alive, build an u-boot image
for your board and place it to an sd card as explained in
several places in this forum. Then you will be able to boot
your u-boot and you can continue loading a Linux image.
Hope this helps.
Sinan Akman