IMX53 CPU :The Block Diagram shows there are 2 camaras Peripheral Interfaces ,but theres is only one csi peripheral,I want to conect 2 camaras ,how?
Hi 王凯 王
please look below
Re: Blurry image with CSI1 overlay
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you!
but there is only one csi (csidata0~csidata19 vsync hsync pix clk ) ,IF I conect two TVP5150 , how ?
I see "
Blurry image with CSI1 overlay
" they use two TVP5150
2014-10-20
wangkai
发件人: igorpadykov
发送时间: 2014-10-20 16:07:01
收件人: 王凯 王
抄送:
主题: Re: - IMX53 CPU :The Block Diagram shows there are2 camaras Peripheral Interfaces ,but theres is o
IMX53 CPU :The Block Diagram shows there are 2 camaras Peripheral Interfaces ,but theres is only one csi peripheral,I want to conect 2 camaras ,how?
reply from igorpadykov in i.MX Community - View the full discussion
Hi 王凯 王
please look below
Re: Blurry image with CSI1 overlay
Best regards
igor
check i.MX53 Reference Manual (rev.2.1 6/2012)
sect.45.3 Features And Functionality
sect.45.3.1 External Ports :
IPU has the following ports:
• Two camera ports - each controlled by a CSI sub-block, providing a connection to
image sensors and related devices.
http://www.freescale.com/files/32bit/doc/ref_manual/iMX53RM.pdf
Table 4-3. Muxing Options sorted by IPs p.340 : ports CSI0,CSI1
~igor