I2S microphone (SPH0645LM4H) Driver Implementation with i.mx6ul with yocto dey2.6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2S microphone (SPH0645LM4H) Driver Implementation with i.mx6ul with yocto dey2.6

4,839 Views
hitesh_kasera
Contributor III

Hi,

 

I am working with 1 I2S microphone (SPH0645LM4H) which is connected to i.MX6UL I2s Interface. I want to record audio from this mems. My device tree set up for the same is:

sound {
compatible = "fsl,imx-audio-sph0645",
"fsl,imx-mic-sph0645";
model = "sph0645-audio";
cpu-dai = <&sai1>;
gpr = <&gpr 4 0x80000 0x80000>;

};

&sai1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_sai1>;
/*
* Reference block.
*
* Codec dependent section.
*/
assigned-clocks = <&clks IMX6UL_CLK_SAI1_SEL>,
<&clks IMX6UL_CLK_SAI1>;
assigned-clock-parents = <&clks IMX6UL_CLK_PLL4_AUDIO_DIV>;
assigned-clock-rates = <0>, <12288000>;
fsl,sai-mclk-direction-output;
status = "okay";

};

i have also attached my driver file for the same.

when i run the command to record audio:

arecord -c 1 -d 5 -f S32 -r 48000 -v /home/root/test.wav

i got below error:

Recording WAVE '/home/root/test.wav' : Signed 32 bit Little Endiafsl-sai 2028000.sai: sampling rate parms_rate output rate : 48000
n, Rate 48000 Hz, Mono
fsl-sai 2028000.sai: bclk : 3072000
fsl-sai 2028000.sai: failed to derive required Rx rate: 3072000
fsl-sai 2028000.sai: ASoC: can't set 2028000.sai hw params: -22
arecord: set_params:1403: Unable to install hw params:
ACCESS:  RW_INTERLEAVED
FORMAT:  S32_LE
SUBFORMAT:  STD
SAMPLE_BITS: 32
FRAME_BITS: 32
CHANNELS: 1
RATE: 48000
PERIOD_TIME: (85333 85334)
PERIOD_SIZE: 4096
PERIOD_BYTES: 16384
PERIODS: 4
BUFFER_TIME: (341333 341334)
BUFFER_SIZE: 16384
BUFFER_BYTES: 65536
TICK_TIME: 0

Request you to please provide inputs, what i might need to change to make it work.

Regards,

Hitesh

Labels (2)
6 Replies

3,498 Views
synaption
Contributor I

This no longer compiles.  sound/soc/fsl/imx-sph0645.c:43:35: error: ‘struct snd_soc_pcm_runtime’ has no member named ‘cpu_dai’
43 | struct snd_soc_dai *cpu_dai = rtd->cpu_dai;

0 Kudos
Reply

4,430 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hitesh

>fsl-sai 2028000.sai: failed to derive required Rx rate: 3072000
>fsl-sai 2028000.sai: ASoC: can't set 2028000.sai hw params: -22

one can try to find reason for these messages debugging sai driver

fsl_sai.c\fsl\soc\sound - linux-imx - i.MX Linux kernel 

and using alsa drivers description in Chapter 7 Audio attached Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,430 Views
hitesh_kasera
Contributor III

Hi Igor,

This is i have asked previously for dey2.4. in there i was not able to receive sai_mclk 12.288Mhz thats the reason now i want to try it on dey2.6 weather it works there or not. i was expecting reply from wigros but still didnt get the response.

i have added same driver file and config to dey2.6 and getting the error.

Request you to please look into this as a reference.

https://community.nxp.com/thread/500755 

Regards,

Hitesh

0 Kudos
Reply

4,430 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hitesh

that thread was already escalated to application team.

If that did not help, suggestion to proceed with help of

NXP Professional Services | NXP 

Best regards
igor

4,430 Views
hitesh_kasera
Contributor III

HI Igor,

Thanks for your response. i will look into that and it will be great if you can help out for dey2.6 driver implementation, if i am missing something in driver file.

It will be really helpful.

Regards,

Hitesh

0 Kudos
Reply

4,430 Views
hitesh_kasera
Contributor III

Hi Igor,

i debugged into driver as you said but still i am getting master clock around 45Hz but in driver its shows 12.288Mhz.

This is the updated driver code:

static int imx_sph0645_hw_params(struct snd_pcm_substream *substream,
        struct snd_pcm_hw_params *params)
{
    struct snd_soc_pcm_runtime *rtd = substream->private_data;
    struct snd_soc_dai *cpu_dai = rtd->cpu_dai;
    u32 channels = 2; //ALWAYS 2 CHANNELS  params_channels(params);
    u32 ratio = 0;
    u64 mclk = 12288000;
    u32 rate = params_rate(params); //sampling rate
        dev_err(cpu_dai->dev, "sampling rate parms_rate output rate : %d \n" , rate);
    u32 bclk = rate * channels * 32; //fixed to sampling rate * 64
//    ratio = mclk / bclk ;    
    ratio = 4;
        dev_err(cpu_dai->dev, "bclk : %d \n" , bclk);    
        dev_err(cpu_dai->dev, "ratio : %d \n" , ratio);
    int ret = 0;

    /* set cpu DAI configuration */
    ret = snd_soc_dai_set_fmt(cpu_dai, SND_SOC_DAIFMT_I2S | SND_SOC_DAIFMT_NB_NF | SND_SOC_DAIFMT_CBS_CFS);
    if (ret) {
        dev_err(cpu_dai->dev, "failed to set dai fmt\n");
        return ret;
    }

    ret = snd_soc_dai_set_tdm_slot(cpu_dai, 0, 3, 2, 32);
    if (ret) {
        dev_err(cpu_dai->dev, "failed to set dai tdm slot\n");
        return ret;
    }

    ret = snd_soc_dai_set_sysclk(cpu_dai, 1, mclk, SND_SOC_CLOCK_OUT);
    if (ret)
        dev_err(cpu_dai->dev, "failed to set cpu sysclk\n");
        return ret;

    ret = snd_soc_dai_set_bclk_ratio(cpu_dai, ratio);
    if (ret)
        dev_err(cpu_dai->dev, "failed to set bclk ratio\n");
    return ret;
}

This is the debugging ouput:

fsl-sai 2028000.sai: Entered into fsl sai set mclk rate mclk_clk[1] = 12288000Hz:
fsl-sai 2028000.sai: Entered into fsl sai set bclk with freq: 3072000 Hz
fsl-sai 2028000.sai: Entered into fsl sai set bclk mclk_clk[0] = 0Hz:
fsl-sai 2028000.sai: Entered into fsl sai set bclk mclk_clk[1] = 12288000Hz:
fsl-sai 2028000.sai: ratio 4 for freq 3072000Hz based on clock 12288000Hz
fsl-sai 2028000.sai: Entered into fsl sai set bclk id and tx : 0, id = 1:
, savediv :4

Request you to provide your inputs regarding master clock setting.

Regards,

Hitesh

0 Kudos
Reply