I2C3 from EPDC Group

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I2C3 from EPDC Group

579件の閲覧回数
pankajrana
Contributor III

Hi,

In the current design we are interfacing a 8 inch EPD, 16 data lines with MCIMX6SLEVK - i.Mx6 SoloLite EVK. The signals "EPDC_SDCE3" and "EPDC_SDCE2" are currently not used. So when we enable the EPDC , is it possible to use these two signals for I2C3 in ALT1 mode ?

--Pankaj Rana

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

425件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Pankaj

yes if not used for EPDC, these pins can be used for other purposes for example

as I2C3 in ALT1 mode.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信