/freeglut-3.2.1# cmake . -DFREEGLUT_WAYLAND=ON
CMake Error at /usr/share/cmake-3.13/Modules/FindPackageHandleStandardArgs.cmak:
Could NOT find OpenGL (missing: OPENGL_opengl_LIBRARY OPENGL_glx_LIBRARY
OPENGL_INCLUDE_DIR)
Call Stack (most recent call first):
/usr/share/cmake-3.13/Modules/FindPackageHandleStandardArgs.cmake:378 (_FPHSA)
/usr/share/cmake-3.13/Modules/FindOpenGL.cmake:395 (FIND_PACKAGE_HANDLE_STAND)
CMakeLists.txt:262 (FIND_PACKAGE)...
This is directly trying to install on board with cmake command.
Board: imx8qxp [4.14.78x]
compiled with thsi command:
bitbake fsl-image-qt5
In case unavailability let me know how to add feature like: libmesa-dev, mesa-common-dev, libglu1-mesa-dev, freeglut3-dev, python3-openGL......
已解决! 转到解答。
Hello Sandeep,
Opengl is available by default in MX8QXP, You need to find the freeglut that are for 64bit libraries.
regards
Can you Plese provide some refrence for adding free-glut to add with yocto with full functionality. i found that glut shared binaries are avaialable at /usr/lib but there is no glut-devel present means headers file are missed [I took installed those headers manually and successfuly compiled].
I have also faced a run time error such as freeglut ( ): OpenGL GLX extension not supported by display ':0'....
how to resolve above issue....If there is some steps missed could you please let me know the right steps to be resolved with refrences or steps....?