I.Mx 6 Dual lite "2 parallel display interface"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I.Mx 6 Dual lite "2 parallel display interface"

878 次查看
muthurajm
Contributor III

Dear all,

Is there a way that we can use TFT Display- 2nos18 bit RGB parallel interface with I.mx6 Dual lite.

Kindly share any details/reference design if you have.

Regards,

Muthuraj M


标签 (1)
2 回复数

771 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Muthuraj

in general this is possible as IPU has two DI inerfaces,

like IPU1_DI0_DISP_CLK, IPU1_DI1_DISP_CLK, please check

Chapter 4 External Signals and Pin Multiplexing  IMX6SDLRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

771 次查看
muthurajm
Contributor III


Hi Igor,

Thanks....Do you have any reference design that used 2 RGB Paralle Interface.

It would be helpfull if any Reference Design Available.

Regards,

Muthuraj M

0 项奖励
回复