I.MX6 Solo power management

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6 Solo power management

Jump to solution
1,079 Views
davidziv
Contributor II

Hello.

I'm new to this processor.

I'm trying to test power consumption.

#echo standby > /sys/power/state

Will this command put the SOM to minimal power consumption?

I have been streaming video

#gst-launch imxv4l2src  capture-mode=4 fps-n=15 ! vpuenc codec=6 ! queue ! rtph264pay ! udpsink host=37.142.163.100 port=5000 -v &

and them tried the

#echo standby > /sys/power/state


The system entered standby, but I didn't see any effect on the current measurement.


Thanks

Labels (3)
0 Kudos
Reply
1 Solution
698 Views
igorpadykov
NXP Employee
NXP Employee

Hi David

suggest to look at AN4715

AN4715, i.MX 6Solo Power Consumption Measurement - Application Note

it shows low power measurement. Note that other peripheral chips may

contribute to figures which you are measuring.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
699 Views
igorpadykov
NXP Employee
NXP Employee

Hi David

suggest to look at AN4715

AN4715, i.MX 6Solo Power Consumption Measurement - Application Note

it shows low power measurement. Note that other peripheral chips may

contribute to figures which you are measuring.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply