I have read the example i.MX6Q PCIe EP/RC Validation System and What is the PCIe i.MX6 max payload size 。but I do not find Code about how to change the TLP size. do you have the test code.??
thank you..
I want to use PCIE transfer data to FPGA,But the I.MX6 SDMA do not Support PCIE. So I use memcpy function to get data From FPGA. FPGA engineer tell me each read request just read 16 Bytes from FPGA,and each write just write 8 bytes.How can I Improve performance ?
follow is PCIe Host config space content:
vendor ID = 0x16c3
device ID = 0xabcd
command register = 0x0007
status register = 0x0010
revision ID = 0x01
class code = 0x06
sub class code = 0x04
programming interface = 0x00
cache line = 0x08
latency time = 0x00
header type = 0x01
BIST = 0x00
base address 0 = 0x01200000
base address 1 = 0x00000000
primary bus number = 0x00
secondary bus number = 0x01
subordinate bus number = 0x01
secondary latency timer = 0x00
IO base = 0xf1
IO limit = 0x01
secondary status = 0x0000
memory base = 0x0100
memory limit = 0x0110
prefetch memory base = 0xfff1
prefetch memory limit = 0x0001
prefetch memory base upper = 0x00000000
prefetch memory limit upper = 0x00000000
IO base upper 16 bits = 0xffff
IO limit upper 16 bits = 0x000f
expansion ROM base address = 0x00000000
interrupt line = 0x9b
interrupt pin = 0x01
bridge control = 0x0000
Capabilities - Power Management
Capabilities - Message Signaled Interrupts: 0x50 control 0x180 Disabled, 64-bit, MME: 0 MMC: 0
Address: 0000000000000000 Data: 0x0000
Per-vector Mask: Support Mask Bit: 0x0, Pending Bit: 0x0
Capabilities - PCIe: Root Port, IRQ 0
Device: Max Payload: 128 bytes, Extended Tag: 5-bit
Acceptable Latency: L0 - <64ns, L1 - <1us
Errors Enabled: Relaxed Ordering
Max Read Request 512 bytes
Link: MAX Speed - 5.0Gb/s, MAX Width - by 1 Port - 0 ASPM - L0s & L1
Latency: L0s - <1us, L1 - <8us
ASPM - Disabled, RCB - 64bytes
Speed - 2.5Gb/s, Width - by 1
Root Control Enabled:
Ext Capabilities - Advanced Error Reporting. 0x100. Version 1. AER Control: 0xa0
Uncorrectable : Mask 0x0. Severity 0x62030
Uncorrectable Status: Correctable : Mask 0x2000.
Correctable Status:
HeaderLog:
Error Source Identification: 0x0 0x0
Ext Capabilities - Virtual Channel. 0x140. Version 1
thanks!!
in suggested link there is example with ipu dma.
There is no SW mechanism to specify the exact number of the bytes in one TLP,
and as answered on https://community.nxp.com/docs/DOC-95014
MAX_PAY_LOAD_SIZE of imx6 pcie is 128bytes.
The actual data size on one tlp is decided by the cache-burst capability of the pcie master.
That's why the data size in the imx6 pcie ep/rc validation is 32 when arm core is used
as the bus master. And the data size is 64 when IPU(DMA) used as the bus master.
Follow the i.MX6Q PCIe EP/RC Validation System ,the test function use TLP Payload size is 8 and 32 Bytes for Write , 32 and 64 for read。if no SW mechanism to specify the exact number of the bytes in one TLP,how did it finish the test?could you give me the test source code?
And cache-burst capability Can not be changed by SW?
thinks!
Hi zhaoping
please look at examples in
i.MX6Q PCIe EP/RC Validation System
What is the PCIe i.MX6 max payload size ?
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------