Hello
I want to use IPU on i.mx6quad from C api but I can not find appropriate header files to do that.
I have searched a lot and now I have got only a big mess in my head.
I know that I need to use ioctl (as it was in ipu examples on github) but with ipu.h file contents I do not know how to use it as CSI 8 bit parallel camera port. It seems that something that I need is in ipu-v3.h file but I can not compile it because there is an error that "resource_size_t does not name a type".
Where can I find or download appropriate headers ?? or where can I find any tutorial with using ipu as 8 bit parallel camera port ?
解決済! 解決策の投稿を見る。
Hi Seba
please check sect.6.3 Source Code Structure attached Linux
Manual, use sources on
http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/?h=imx_4.1.15_1.0.0_ga
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thak You ! That was exactly what I was looking for.
But I am a linux newbie and my folder mxc/ipu3 contains only Makefile and Kconfig file - nothing else.
Is there a possibility to use this libraries in debian or only in Yocto project ??
Hi Seba
please check sect.6.3 Source Code Structure attached Linux
Manual, use sources on
http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/?h=imx_4.1.15_1.0.0_ga
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------