[I.MX6 DL]Calibrate accuracy of RTC clock for temp drift

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[I.MX6 DL]Calibrate accuracy of RTC clock for temp drift

1,161 Views
yuji_fuseki
Contributor II

Hi, 

Now, we use i.MX6 Dual lite, and going to use SRTC function.

Does this SoC have the function to calibrate RTC clock(that is provided from external crystal) accuracy in temp drift point of view?

(It is like TCXO function)

br,

yuji

Labels (1)
Tags (2)
3 Replies

1,075 Views
yuji_fuseki
Contributor II

Hi Karan,

Thanks for your reply.

Regarding this "Calibrating time counter", this function can be calibrate drift which is caused by temperature?

Br,

Yuji

0 Kudos

1,075 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Yuji,

In fact, the time drift of the RTC is determined by the temperature drift curve of the external crystal. To fundamentally solve this problem, RTC time compensation needs to be performed according to the temperature drift curve of the external 32.768K crystal. Therefore, the best way is to ask the crystal manufacturer if there is a corresponding plan. For example, if you use EPSON crystals, you need to contact EPSON.

Hope the information is helpful to you.

Have a nice day!

B.R,

Weidong

1,075 Views
karangajjar
Senior Contributor II

Hi Yuji Fuseki ,

Please refer to the iMX6DL Reference Manual Chapter 57: Secure Non-Voltage Storage(SNVS).

You will find a section for "Calibrating the time counter" and SNVS Memory Map/Register Definition for the same.

Regards,

Karan Gajjar

0 Kudos