Hi All,
I am getting this message continuously at start up. Please help.
starting pid 1129, tty '': '/sbin/getty -L ttymxc0 115200 vt100'
process '/sbin/getty -L ttymxc0 115200 vt100' (pid 1129) exited. Scheduling for restart.
When you post a question, please, be aware of giving us at least some basic information. Something like:
* board used
* BSP you´ve been using (is it linux? android? ubuntu?)
* what´s the kernel version
* what was the changes you made.
* are you booting from SDCard? From SPInor? From NFS?
* what´s the bootargs/kernel command line?
Hi,
Sorry for providing incomplete info. Below are the details,
* I.MX53 QSB
* Linux 2.6.31
* changed the boot options in kernel (using menu config) to --> noinitrd console=ttymxc0 115200 root=/dev/mmblk0p1 rw rootfstype=ext2 ( Before it was set to root=/dev/mtd...)
* using tftpboot to transfer the image file and rfs is on the sdcard
Log:
Starting kernel ... | |
Uncompressing Linux.............................................................
Linux version 2.6.31-506-g30df573 (user@user) (gcc v2
MXC_Early serial console at MMIO 0x43f90000 (options '115200') | |
console [ttymxc0] enabled | |
Console: colour dummy device 80x30 | |
Calibrating delay loop... 530.84 BogoMIPS (lpj=2654208) | |
Mount-cache hash table entries: 512 |
CPU: Testing write buffer coherency: ok
usb: Host 2 host (serial) registered | |
usb: DR host (utmi) registered | |
usb: DR gadget (utmi) registered | |
JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc. | |
msgmni has been set to 245 | |
io scheduler noop registered | |
io scheduler anticipatory registered | |
io scheduler deadline registered | |
io scheduler cfq registered (default) | |
mxc_ipu mxc_ipu: Channel already uninitialized 14 | |
Console: switching to colour frame buffer device 30x20 | |
mxc_ipu mxc_ipu: Channel already uninitialized 15 | |
mxcfb: fb registered, using mode <NULL> | |
regulator: get() with no identifier | |
Serial: MXC Internal UART driver | |
mxcintuart.0: ttymxc0 at MMIO 0x43f90000 (irq = 45) is a Freescale i.MX | |
console handover: boot [ttymxc0] -> real [ttymxc0] | |
mxcintuart.1: ttymxc1 at MMIO 0x43f94000 (irq = 32) is a Freescale i.MX | |
mxcintuart.2: ttymxc2 at MMIO 0x5000c000 (irq = 18) is a Freescale i.MX | |
loop: module loaded | |
MXC MTD nor Driver 2.0 |
Linux video capture interface: v2.00 | |
MXC Video Output MXC Video Output.0: Registered device video0 | |
MXC WatchDog Driver 2.0 | |
MXC Watchdog # 0 Timer: initial timeout 60 sec | |
IPU Post-filter loading | |
ioctl pointer: c0260188. mmap pointer: c025fc8c | |
RNG Driver: Loading | |
mxc_asrc registered | |
sdhci: Secure Digital Host Controller Interface driver | |
sdhci: Copyright(c) Pierre Ossman | |
mxsdhci: MXC Secure Digital Host Controller Interface driver | |
mxsdhci: MXC SDHCI Controller Driver. | |
mmc0: SDHCI detect irq 242 irq 7 INTERNAL DMA | |
mxsdhci: MXC SDHCI Controller Driver. | |
mmc1: SDHCI detect irq 0 irq 8 INTERNAL DMA | |
Advanced Linux Sound Architecture Driver Version 1.0.20. | |
regulator: Unable to get requested regulator: VDDIO | |
regulator: Unable to get requested regulator: VDDD | |
sgtl5000-i2c 0-000a: SGTL5000 revision 17 | |
i2c-adapter i2c-0: ACK not received | |
ak4647_read_reg:read reg errorr:reg=0,val=ffffff87 | |
Device with ID register 0 is not a AK4647 | |
DMA Sound Buffers Allocated:UseIram=1 buf->addr=10001000 buf->area=c8841000 siz6 |
DMA Sound Buffers Allocated:UseIram=1 buf->addr=87cb0000 buf->area=fde01000 siz6
asoc: SGTL5000 <-> imx-ssi-1-0 mapping ok | |
imx-3stack-ak4647: probe of imx-3stack-ak4647.0 failed with error -16 |
DMA Sound Buffers Allocated:UseIram=1 buf->addr=0 buf->area=b8840000 size=65536
asoc: WM8580 PAIFRX <-> imx-esai-txrx mapping ok | |
ASoC: Failed to create codec register debugfs file | |
Failed to create pop time debugfs file |
DMA Sound Buffers Allocated:UseIram=1 buf->addr=87cc0000 buf->area=fde11000 siz6
DMA Sound Buffers Allocated:UseIram=1 buf->addr=87cf0000 buf->area=fde21000 siz6
asoc: bluetooth <-> imx-ssi-2-0 mapping ok | |
ASoC: Failed to create codec register debugfs file |
Failed to create pop time debugfs file
input: mxc_ts as /class/input/input1 | |
mxc input touchscreen loaded | |
pmic_rtc pmic_rtc.1: setting system clock to 1970-01-01 00:00:59 UTC (59) | |
Waiting 10sec before mounting root device... | |
mmc0: new SDHC card at address aaaa | |
mmcblk0: mmc0:aaaa SD04G 3.69 GiB | |
mmcblk0: p1 | |
EXT2-fs warning: mounting unchecked fs, running e2fsck is recommended | |
VFS: Mounted root (ext2 filesystem) on device 179:1. | |
Freeing init memory: 104K | |
init started: BusyBox v1.15.0 () | |
starting pid 1046, tty '': '/etc/rc.d/rcS' | |
Mounting /proc and /sys | |
Starting the hotplug events dispatcher udevd |
udevd[1054]: init_udevd_socket: error getting socket: Address family not supporl
error initializing udevd socket | |
udevd[1054]: main: error initializing udevd socket | |
Synthesizing initial hotplug events | |
Setting the hostname to freescale | |
Mounting filesystems | |
Starting inetd: | |
starting pid 1099, tty '': '/sbin/getty -L ttymxc0 115200 vt100' |
process '/sbin/getty -L ttymxc0 115200 vt100' (pid 1099) exited. Scheduling for.
starting pid 1124, tty '': '/sbin/getty -L ttymxc0 115200 vt100' |
process '/sbin/getty -L ttymxc0 115200 vt100' (pid 1124) exited. Scheduling for.
starting pid 1127, tty '': '/sbin/getty -L ttymxc0 115200 vt100' |
process '/sbin/getty -L ttymxc0 115200 vt100' (pid 1127) exited. Scheduling for.
starting pid 1130, tty '': '/sbin/getty -L ttymxc0 115200 vt100' |
process '/sbin/getty -L ttymxc0 115200 vt100' (pid 1130) exited. Scheduling for.
starting pid 1133, tty '': '/sbin/getty -L ttymxc0 115200 vt100'
Bootargs:
bootdelay=3
baudrate=115200
loadaddr=0x80800000
netdev=eth0
ethprime=smc911x
uboot_addr=0xa0000000
uboot=u-boot.bin
kernel=uImage
nfsroot=/opt/eldk/arm
bootargs_nfs=setenv bootargs ${bootargs} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp
bootcmd_net=run bootargs_base bootargs_nfs; tftpboot ${loadaddr} ${kernel}; bootm
prg_uboot=tftpboot ${loadaddr} ${uboot}; protect off ${uboot_addr} 0xa003ffff; erase ${uboot_addr} 0xa003ffff; cp.b ${loadaddr} ${uboot_addr}v
ethact=smc911x-0
bootargs_base=setenv bootargs console=ttymxc0,115200
bootcmd_nand=run bootargs_base bootargs_nand; cp 0xa0080000 ${loadaddr} 0x300000;bootm
bootargs_nand=setenv bootargs ${bootargs} console=tty0 root=/dev/mmcblk0p1 rootdelay=10 rw
filesize=1FFF18
fileaddr=80800000
ipaddr=192.168.42.32
serverip=192.168.42.1
bootcmd_tftp=console=ttymxc0,115200 root=/dev/mmcblk0p1 rootdelay=10 rw;tftpboot 0x80100000 uImage;bootm
bootargs=console=ttymxc0,115200 root=/dev/mmcblk0p1 rootdelay=10 rw
bootcmd=run bootcmd_tftp
stdin=serial
stdout=serial
stderr=serial
How did you created the rootfs?
I have never saw this error for FSL prebuilt image. But I did when I was working with a systemD rootfs and a uncompatible kernel.
And, why are you using 2.6.31 kernel? Please, take a look in the following link and see if you are able to use 2.6.35 kernel (this is latest supported kernel)
http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/log/?h=imx_2.6.35_11.09.01
Thanks for the quick reply.
Once ltib has generated a image and rfs ... i use the below commands to copy the rfs to sd card on my host
umount /media/xyz
mkfs -t ext2 /dev/sdb1
mkdir /mnt/sd
mount /dev/sdb1 /mnt/sd
cp -pr rootfs/* /dev/sdb1
I could see one more person having the same issues in the below post:
Hi,
Can anyone please help... stuck at this point.... not sure where i am going wrong.
Thanks.