I.MX53 not able to reach the root prompt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX53 not able to reach the root prompt

1,843 Views
abdulrazak
Contributor I

Hi All,


I am getting this message continuously at start up. Please help.


starting pid 1129, tty '': '/sbin/getty -L ttymxc0 115200 vt100'

process '/sbin/getty -L ttymxc0 115200 vt100' (pid 1129) exited. Scheduling for restart.


Labels (1)
0 Kudos
6 Replies

936 Views
daiane_angolini
NXP Employee
NXP Employee

When you post a question, please, be aware of giving us at least some basic information. Something like:

* board used

* BSP you´ve been using (is it linux? android? ubuntu?)

* what´s the kernel version

* what was the changes you made.

* are you booting from SDCard? From SPInor? From NFS?

* what´s the bootargs/kernel command line?

0 Kudos

936 Views
abdulrazak
Contributor I

Hi,

Sorry for providing incomplete info. Below are the details,

* I.MX53 QSB

* Linux 2.6.31

* changed the boot options in kernel (using menu config) to --> noinitrd console=ttymxc0 115200 root=/dev/mmblk0p1 rw rootfstype=ext2 ( Before it was set to root=/dev/mtd...)

* using tftpboot to transfer the image file and rfs is on the sdcard

Log:

Starting kernel ...                                                      

Uncompressing Linux.............................................................

Linux version 2.6.31-506-g30df573 (user@user) (gcc v2

MXC_Early serial console at MMIO 0x43f90000 (options '115200')           
console [ttymxc0] enabled                                                
Console: colour dummy device 80x30                                       
Calibrating delay loop... 530.84 BogoMIPS (lpj=2654208)                  
Mount-cache hash table entries: 512                                      

CPU: Testing write buffer coherency: ok

usb: Host 2 host (serial) registered                                     
usb: DR host (utmi) registered                                           
usb: DR gadget (utmi) registered                                         
JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.                     
msgmni has been set to 245                                               
io scheduler noop registered                                             
io scheduler anticipatory registered                                     
io scheduler deadline registered                                         
io scheduler cfq registered (default)                                    
mxc_ipu mxc_ipu: Channel already uninitialized 14                        
Console: switching to colour frame buffer device 30x20                   
mxc_ipu mxc_ipu: Channel already uninitialized 15                        
mxcfb: fb registered, using mode <NULL>                                  
regulator: get() with no identifier                                      
Serial: MXC Internal UART driver                                         
mxcintuart.0: ttymxc0 at MMIO 0x43f90000 (irq = 45) is a Freescale i.MX  
console handover: boot [ttymxc0] -> real [ttymxc0]                       
mxcintuart.1: ttymxc1 at MMIO 0x43f94000 (irq = 32) is a Freescale i.MX  
mxcintuart.2: ttymxc2 at MMIO 0x5000c000 (irq = 18) is a Freescale i.MX  
loop: module loaded                                                      
MXC MTD nor Driver 2.0                     
Linux video capture interface: v2.00                                     
MXC Video Output MXC Video Output.0: Registered device video0            
MXC WatchDog Driver 2.0                                                  
MXC Watchdog # 0 Timer: initial timeout 60 sec                           
IPU Post-filter loading                                                  
ioctl pointer: c0260188.  mmap pointer: c025fc8c                         
RNG Driver: Loading                                                      
mxc_asrc registered                                                      
sdhci: Secure Digital Host Controller Interface driver                   
sdhci: Copyright(c) Pierre Ossman                                        
mxsdhci: MXC Secure Digital Host Controller Interface driver             
mxsdhci: MXC SDHCI Controller Driver.                                    
mmc0: SDHCI detect irq 242 irq 7 INTERNAL DMA                            
mxsdhci: MXC SDHCI Controller Driver.                                    
mmc1: SDHCI detect irq 0 irq 8 INTERNAL DMA                              
Advanced Linux Sound Architecture Driver Version 1.0.20.                 
regulator: Unable to get requested regulator: VDDIO                      
regulator: Unable to get requested regulator: VDDD                       
sgtl5000-i2c 0-000a: SGTL5000 revision 17                                
i2c-adapter i2c-0: ACK not received                                      
ak4647_read_reg:read reg errorr:reg=0,val=ffffff87                       
Device with ID register 0 is not a AK4647                                
DMA Sound Buffers Allocated:UseIram=1 buf->addr=10001000 buf->area=c8841000 siz6

DMA Sound Buffers Allocated:UseIram=1 buf->addr=87cb0000 buf->area=fde01000 siz6

asoc: SGTL5000 <-> imx-ssi-1-0 mapping ok                                
imx-3stack-ak4647: probe of imx-3stack-ak4647.0 failed with error -16    

DMA Sound Buffers Allocated:UseIram=1 buf->addr=0 buf->area=b8840000 size=65536

asoc: WM8580 PAIFRX <-> imx-esai-txrx mapping ok                         
ASoC: Failed to create codec register debugfs file                       
Failed to create pop time debugfs file                                   

DMA Sound Buffers Allocated:UseIram=1 buf->addr=87cc0000 buf->area=fde11000 siz6

DMA Sound Buffers Allocated:UseIram=1 buf->addr=87cf0000 buf->area=fde21000 siz6

asoc: bluetooth <-> imx-ssi-2-0 mapping ok                               
ASoC: Failed to create codec register debugfs file                       

Failed to create pop time debugfs file

input: mxc_ts as /class/input/input1                                     
mxc input touchscreen loaded                                             
pmic_rtc pmic_rtc.1: setting system clock to 1970-01-01 00:00:59 UTC (59)
Waiting 10sec before mounting root device...                             
mmc0: new SDHC card at address aaaa                                      
mmcblk0: mmc0:aaaa SD04G 3.69 GiB                                        
mmcblk0: p1                                                             
EXT2-fs warning: mounting unchecked fs, running e2fsck is recommended    
VFS: Mounted root (ext2 filesystem) on device 179:1.                     
Freeing init memory: 104K                                                
init started: BusyBox v1.15.0 ()                                         
starting pid 1046, tty '': '/etc/rc.d/rcS'                               
Mounting /proc and /sys                                                  
Starting the hotplug events dispatcher udevd                             

udevd[1054]: init_udevd_socket: error getting socket: Address family not supporl

error initializing udevd socket                                          
udevd[1054]: main: error initializing udevd socket                       
Synthesizing initial hotplug events                                      
Setting the hostname to freescale                                        
Mounting filesystems                                                     
Starting inetd:                                                          
starting pid 1099, tty '': '/sbin/getty -L ttymxc0 115200 vt100'         

process '/sbin/getty -L ttymxc0 115200 vt100' (pid 1099) exited. Scheduling for.

starting pid 1124, tty '': '/sbin/getty -L ttymxc0 115200 vt100'         

process '/sbin/getty -L ttymxc0 115200 vt100' (pid 1124) exited. Scheduling for.

starting pid 1127, tty '': '/sbin/getty -L ttymxc0 115200 vt100'         

process '/sbin/getty -L ttymxc0 115200 vt100' (pid 1127) exited. Scheduling for.

starting pid 1130, tty '': '/sbin/getty -L ttymxc0 115200 vt100'         

process '/sbin/getty -L ttymxc0 115200 vt100' (pid 1130) exited. Scheduling for.

starting pid 1133, tty '': '/sbin/getty -L ttymxc0 115200 vt100'

Bootargs:

bootdelay=3

baudrate=115200

loadaddr=0x80800000

netdev=eth0

ethprime=smc911x

uboot_addr=0xa0000000

uboot=u-boot.bin

kernel=uImage

nfsroot=/opt/eldk/arm

bootargs_nfs=setenv bootargs ${bootargs} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp

bootcmd_net=run bootargs_base bootargs_nfs; tftpboot ${loadaddr} ${kernel}; bootm

prg_uboot=tftpboot ${loadaddr} ${uboot}; protect off ${uboot_addr} 0xa003ffff; erase ${uboot_addr} 0xa003ffff; cp.b ${loadaddr} ${uboot_addr}v

ethact=smc911x-0

bootargs_base=setenv bootargs console=ttymxc0,115200

bootcmd_nand=run bootargs_base bootargs_nand; cp 0xa0080000 ${loadaddr} 0x300000;bootm

bootargs_nand=setenv bootargs ${bootargs} console=tty0 root=/dev/mmcblk0p1 rootdelay=10 rw

filesize=1FFF18

fileaddr=80800000

ipaddr=192.168.42.32

serverip=192.168.42.1

bootcmd_tftp=console=ttymxc0,115200 root=/dev/mmcblk0p1 rootdelay=10 rw;tftpboot 0x80100000 uImage;bootm

bootargs=console=ttymxc0,115200 root=/dev/mmcblk0p1 rootdelay=10 rw

bootcmd=run bootcmd_tftp

stdin=serial

stdout=serial

stderr=serial


0 Kudos

936 Views
daiane_angolini
NXP Employee
NXP Employee

How did you created the rootfs?

I have never saw this error for FSL prebuilt image. But I did when I was working with a systemD rootfs and a uncompatible kernel.

And, why are you using 2.6.31 kernel? Please, take a look in the following link and see if you are able to use 2.6.35 kernel (this is latest supported kernel)

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/log/?h=imx_2.6.35_11.09.01

936 Views
abdulrazak
Contributor I

Thanks for the quick reply.

Once ltib has generated a image and rfs ... i use the below commands to copy the rfs to sd card on my host

umount  /media/xyz

mkfs -t ext2 /dev/sdb1

mkdir /mnt/sd

mount /dev/sdb1 /mnt/sd

cp -pr rootfs/* /dev/sdb1

I could see one more person having the same issues in the below post:

mx53qsb ERROR "cp: write error: No space left on device"

0 Kudos

936 Views
davee
Contributor III

Hi

Have you solved your original problem of getty respawning.

Cheers,

Dave

0 Kudos

936 Views
abdulrazak
Contributor I

Hi,

Can anyone please help... stuck at this point.... not sure where i am going wrong.

Thanks.

0 Kudos