Hello,
i can build a imx6qsabrelite fsl-image-machine-test image. When i add to IMAGE_FSTYPES the value "sdcard" it builds me sdcard images. But u-boot is missing on the sdcard image.
I tried adding IMAGE_BOOTLOADER = "u-boot" and SDCARD= "/dev/sdd" to the bitbake variables but u-boot is still missing.
I tried also alot of other vars like UBOOT_CONFIG and so on, but no luck.
What do i need to build a sdcard image with u-boot included ? It seemed that there is also a way to directly write the sdcard image after build ? If thats possible, what do i need todo to enable this ?
if you need to write uboot image to sdcard, you can use mfgtools or dd command in the linux.
for mfgtools, you can download from nxp official website, if you couldn't find it, pls tell me your bsp version, I can send the link to you. if you want to use dd command, you can use "$ sudo dd if=<U-Boot image> of=/dev/sd<partition> bs=512 seek=2 conv=fsync"
thanks, but i mean a bitbake variable that triggers a function that will directly build the sdcard image with u-boot installed. I see in _toaster_clones/_git___github.com_Freescale_meta-fsl-arm-extra.git_morty/conf/machine/nitrogen6x.conf that the bitbake var IMAGE_BOOTLOADER is empty. If i set IMAGE_BOOTLOADER to "u-boot" it still does not build a sdcard image with u-boot included, so what do i need extra ? Set IMAGE_BOOT_FILES ? or is this automatically set anywhere ?