Hi,
How to support QT5 applications based on X11 or wayland backend in imx7d Sabre board?
the software version: fsl-yocto-L4.1.15_1.2.0-ga
First, I made qt5 sdk using the command "bitbake meta-toolchain-qt5", installed the SDK package,
then compiled QT project, but can't work well.
source /opt/fsl-imx-wayland-tcqt5/4.1.15-2.0.0/environment-setup-cortexa7hf-neon-poky-linux-gnueabi
developer@developer-T440 ~/qt5/examples/gui/analogclock $ qmake analogclock.pro
Cannot read /opt/fsl-imx-wayland-tcqt5/4.1.15-2.0.0/sysroots/cortexa7hf-neon-poky-linux-gnueabi/usr/lib/qt5/mkspecs/oe-device-extra.pri: No such file or directory
Would you like to give me some advice? Thanks a lot in advance!
Regards,
Jiang
解決済! 解決策の投稿を見る。
Hi Jiang
please check
[meta-freescale] [meta-fsl-arm PATCH v3 17/17] qtbase: Enable support for i.MX SoCs with PXP
as for nxp L4.1.15_1.2.0 there was no formal testing or support for QT, please check
attached Release Notes sect.2.1 New features
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Jiang
please check
[meta-freescale] [meta-fsl-arm PATCH v3 17/17] qtbase: Enable support for i.MX SoCs with PXP
as for nxp L4.1.15_1.2.0 there was no formal testing or support for QT, please check
attached Release Notes sect.2.1 New features
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Ok, Thanks a lot!