How to sign the ssp polarity rom patch?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to sign the ssp polarity rom patch?

936 Views
weo
Contributor I

For a secure boot from SD on a i.MX28 it is necessary to sign the ssp polarity rom patch that is put into the eeprom.

In principle, it is easy. But:

The patch is loaded to address 0xe400 and that is a reserved memory area. HAB gives an error with reason 0x22, "invalid address: access denied". The secure boot fails.

If I load the patch to a different address, for example 0x8000, I get random crashes, I guess because of uninitialized memory (because the patch is not position independent??)

I'd appreciate any help!

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

785 Views
b36401
NXP Employee
NXP Employee

You need to rebuild HAB data with adding this patch.

You can refer to chapter 3.3 of Secure Boot with i.MX28 HAB Version 4 Application Note:

http://cache.freescale.com/files/32bit/doc/app_note/AN4555.pdf

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

785 Views
weo
Contributor I

Thank you for you repsonse!

I did sign the patch. I had to put the signature before the patch because the area at 0xe400 is only 4KB followed by the private data of the rom monitor.

I get these HAB events:

HAB Status: 0x000000f0, 0x000000f0 [0x33]

--------- HAB Event 1 -----------------

event data:

    0xdb 0x00 0x14 0x40 0x33 0x22 0x33 0x00

    0x00 0x00 0x00 0x0f 0x00 0x00 0xe3 0x98

    0x00 0x00 0x00 0x80

--------- HAB Event 2 -----------------

event data:

    0xdb 0x00 0x14 0x40 0x33 0x22 0x33 0x00

    0x00 0x00 0x00 0x0f 0x00 0x00 0xe4 0x18

    0x00 0x00 0x00 0x80

--------- HAB Event 3 -----------------

event data:

    0xdb 0x00 0x14 0x40 0x33 0x22 0x33 0x00

    0x00 0x00 0x00 0x0f 0x00 0x00 0xe4 0x98

    0x00 0x00 0x00 0x80

...

Best regards,

Wolfgang

0 Kudos
Reply