Hi I'm working on the fuse configuration to boot from my raw NAND (MT29F4G08ABAEA), but I'm confused if I have to set the two NAND_READ_CMD_CODE fields. Do I need to burn this fuses and if Yes to what value (Read Page --> 0x00 and 0x30 ?).
I have already set the following fuses:
0x05 (b00,w05) 0x0450 OCOTP_CFG4 = 0x00001280
CFG1 = NAND, raw, 1 Device, 3 row address bytes (nedds to be 5 row?)
CFG2 = Block has 64 Pages, BOOT_SEARCH_CONT = 4
CFG3 = not used
CFG4 = not used
0x06 (b00,w06) 0x0460 OCOTP_CFG5 = 0x00000010
(BT_FUSE_SEL = 1)
Con You please help me to set
0x07 (b00,w07) 0x0470 OCOTP_CFG6
thanks
Martin
Hi Martin
nand boot will work fine without changing default NAND_READ_CMD_CODE fields.
They can be used for some non-standard cases.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------