we are developing the BSP of iMX6D : MCIMX6D5EYM10ad SBOX1519, and we can boot the u-boot and kernel in our board now;
but we just change the CPU of our board, and change it to iMX6DL : MCIMX6U5EVM10AC XAC1551, other parts keep no change.
could you tell me how to porting uboot and kernel from iMX6D to iMX6DL?
is there a user guide? or some practices?
thanks in advance!
Hi,
Could you tell me which BSP are you using?
Have a nice day
Rita
we are using the Q7 board of Advantech, and get the initial BSP from them;
the kernel version is 4.1-r0, the u-boot version is v2016.07+gitAUTOINC+ae973bc45d-r0;
and use Yokto to compile the BSP;
i don't find the exact version of this BSP, could you tell me how to look at the version?
thanks
Hi,
Here you are using the board from Advantech, details design and porting you can contact them. In our website there're i.MX_BSP_Porting_Guide.pdf and Freescale_Yocto_Project_User's_Guide.pdfdocument for custom. You can refer to .
Hope this can help you
Have a great day,
Rita
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Which BSP you are using?
we are using the Q7 board of Advantech, and get the initial BSP from them;
the kernel version is 4.1-r0, the u-boot version is v2016.07+gitAUTOINC+ae973bc45d-r0;
and use Yokto to compile the BSP;
Hi yn zheng,
You need to get iMX6DL environment setup from Advantech. And then you can able to build for iMX6DL.
For your reference: