HI
I'm trying to bring up the bluetooth SCO voice over PCM.
I had create a sound card for PCM(SAI2) on IMX8. (SAI2 PCM connect to BT chip)
And I can get the waveform while "aplay -D plughw:3,0 test.wav" (bluetooth sound card is 3) on SAI2.
But how do I play the music over SCO PCM to BT headset?
I'm using Yocto system and the version is "i.MX Linux Yocto Project BSP 5.4.3_1.0.0 Release".
And the bluez version is "bluetoothctl: 5.50".
Thanks
What's great about music and klingeltöne can all be found easily. Thank you for these interesting sharing
I think right, in general nxp official documentation on below link
(Release Notes, Linux Manual) does not mention it
i.MX Software and Development Tools | NXP
Best regards
igor
HI igorpadykov
We change the OS to android.
And we use tinyplay to play .wav file to PCM interface(SAI2).
We can see the waveform on the scope, there is clk, sync and output data(TX).
Then we set the BT module to PCM loopback mode.
After set the BT module to PCM loopback mode, we can see the input data on PCM RX.
But when we use tinycap to record the RX data, we just got the .wav file header with dummy data(0).
Did I miss any setting on the audio driver or device tree. I can provide the partial code if you need it for debug.
Thanks
Hi Jimi
wifi/bluetooth documenation can be found on:
wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html
and may be useful to look on
i.MX8M EVK Bluetooth HSP (SCO) audio
also for SCO PCM bluetooth special firmware may be required as mentioned on vendor portal
Murata BCM4339 ZP Bluetooth /Wifi Module - PCM ... | Cypress Developer Community
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------