Hello All,
I would like to reserve more free RAM space for running applications. My idea is to make the kernel and Android code size smaller by removing un-desired features and drivers. For kernel, I can use "make menuconfig" to configure it. For Android, does it offer any configure options?
My another question is in kernel, devices "pmem_adsp" and "pmem_gpu" are created for the Android. How to determine the required size to these pmem devices? Can I make these size smaller?
My BSP release is i.MX50 R10.3.
Thanks,
Peter
已解决! 转到解答。
hello, all:
Suggest that you can work out one memory layout according to your feature lists.
We have put one memory optimization example for MX53 under
https://community.freescale.com/docs/DOC-93334
Hope it's helpful.
You can customize the file ./imx50_rdp/required_hardware.xml to remove those feature you dont need in android framework.
And remove those service/daemon you dont need in init.rc
"pmem_adsp": is use as a physical-continuous buffer allocator for hardware video decoder and encoder. Since there is no vpu in mx50, you can remove the pmem_adsp in kernel
"pmem_gpu": is use as the physical-continuous buffer allocator for the android hal Gralloc. Android framework use the allocator to allocate the buffer for UI surface. It is highly dependents on your device display's resolution.
The size >= 5* display_w × display_h *sizeof(RGBA8888) * 2
Hi Guoyin, Xiaoli
About pmem_gpu, it seem that your formula is not consistent.
Maybe 5 layers is the maximum layers in practical, and 31 is theoretical maximum, is it?
which one you recommend
Thanks
Yes, you are right about the max layers Andorid framework may have. But in practice, we never see the user case you have more than 5. And considering not all the layer has the same size of display resolution and the memory fragment in the pmem_gpu, you may need to set the layers number be greater than 5. A safety number can be 8~10, i guess.
hello, all:
Suggest that you can work out one memory layout according to your feature lists.
We have put one memory optimization example for MX53 under
https://community.freescale.com/docs/DOC-93334
Hope it's helpful.
Hi Xiaoli,
Our environment:
800*480 display resolution,
Support 720P
Not support dual display
About vpu pmem, your formula: 1920*1080*1.5*19=56M, according to our project: 1280*720*1.5*19=26265600.
So, is 32M enough? does mem fragment influence it?
Thanks