Hello all ,
I met a strange problem when i use Ltib and customized linaro tool chain to build my project.
To my project, i need to use newer linaro toolchain to replace the gcc-4.6.2 (glibc2.13).
After i modify the configure option [ Toolchain , ToolchainPath and CFLAGS) and rebuild my project, i found the compile process is halted at .Processing: base_libs. Before that, the linux kernel is compiled successfully.
Processing: base_libs
=======================
Build path taken because: no prebuilt rpm,
....
....
....
sudo /opt/freescale/ltib/usr/bin/rpm --root /home/cyabc/ltib/rootfs --dbpath /var/lib/rpm -e --allmatches --nodeps --define '_tmppath /tmp/ltib' base_libs 2>/dev/null
sudo /opt/freescale/ltib/usr/bin/rpm --root /home/cyabc/ltib/rootfs --dbpath /var/lib/rpm --prefix / --ignorearch -ivh --force --excludedocs --define '_tmppath /tmp/ltib' /home/cyabc/ltib/rpm/RPMS/arm/base_libs-1.2-1.arm.rpm
error: failed dependencies:
ld-linux.so.3(GLIBC_2.4) is needed by base_libs-1.2-1
f_buildrpms() returned an error, exiting
traceback:
main:572
Started: Fri Jun 14 20:57:47 2013
Ended: Fri Jun 14 21:17:12 2013
Elapsed: 1165 seconds
Build Failed
I have attched the error log in attachment file. Could anyone can help to resolve this problem
Original Attachment has been moved to: ltib_build_logt.txt.zip
已解决! 转到解答。
Please refer to the link http://sourceware.org/ml/crossgcc/2012-09/msg00069.html. It maybe helpful for you to resolve the problem.
Please refer to the link http://sourceware.org/ml/crossgcc/2012-09/msg00069.html. It maybe helpful for you to resolve the problem.