imx6 hdmi 576i output

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 hdmi 576i output

1,359件の閲覧回数
ajaykumar
Contributor I

Is it possible to configure imx HDMI to 576i mode to use tv encoder on HDMI port. We want to use HDMI to connect to TV encoder IC to generate PAL signal.

ラベル(4)
0 件の賞賛
返信
1 返信

1,034件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ajay

please look at HDMI supported formats IMX6DQRM

Table 33-3. Video Modes and row : "720(1440)x576i (SDTV)".

One can check below link for examples of interlaced formats

Patch for iMX6 BSP to support interlaced display on HDMI and LCD interface

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信