Hello all ,
I met a strange problem when i use Ltib and customized linaro tool chain to build my project.
To my project, i need to use newer linaro toolchain to replace the gcc-4.6.2 (glibc2.13).
After i modify the configure option [ Toolchain , ToolchainPath and CFLAGS) and rebuild my project, i found the compile process is halted at .Processing: base_libs. Before that, the linux kernel is compiled successfully.
Processing: base_libs
=======================
Build path taken because: no prebuilt rpm,
....
....
....
sudo /opt/freescale/ltib/usr/bin/rpm --root /home/cyabc/ltib/rootfs --dbpath /var/lib/rpm -e --allmatches --nodeps --define '_tmppath /tmp/ltib' base_libs 2>/dev/null
sudo /opt/freescale/ltib/usr/bin/rpm --root /home/cyabc/ltib/rootfs --dbpath /var/lib/rpm --prefix / --ignorearch -ivh --force --excludedocs --define '_tmppath /tmp/ltib' /home/cyabc/ltib/rpm/RPMS/arm/base_libs-1.2-1.arm.rpm
error: failed dependencies:
ld-linux.so.3(GLIBC_2.4) is needed by base_libs-1.2-1
f_buildrpms() returned an error, exiting
traceback:
main:572
Started: Fri Jun 14 20:57:47 2013
Ended: Fri Jun 14 21:17:12 2013
Elapsed: 1165 seconds
Build Failed
I have attched the error log in attachment file. Could anyone can help to resolve this problem
Original Attachment has been moved to: ltib_build_logt.txt.zip
解決済! 解決策の投稿を見る。
Please refer to the link http://sourceware.org/ml/crossgcc/2012-09/msg00069.html. It maybe helpful for you to resolve the problem.
are you solver this problem?
Please refer to the link http://sourceware.org/ml/crossgcc/2012-09/msg00069.html. It maybe helpful for you to resolve the problem.
platform is i.mx6
os is linux3.0.35
Jun Sun, please click Correct Answer/Helpful Answer if your question had been answered.
Thanks,
Yixing
Dear Jun Sun, Freescale does not support other toochain and you may need to get help from somewhere else.
Thanks,
Yixing
Jun Sun, please specify which platform you are working on?
Thanks,
Yixing