How to enable the hdmi for imx6dl custom board with lvds-hdmi bridge chip

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to enable the hdmi for imx6dl custom board with lvds-hdmi bridge chip

937 次查看
bit-hauer
Contributor I

Hi nxp-community,

we have a custom board on which supports an imx6dl som and has got implemented a lvds-hdmi bridge chip (it6263).

I have adapted the device tree, added video command to uboot and configured the CONFIG_DRM_ITE_IT6263=y. Also all DRM and SIMPLE_PANEL config switches are enabled. The bridge chip is recognized by the it6263 driver - but that's it then.
It seems that imx-ldb register function, which should attache the bridge, is not called during startup. mxc_sdc fb instead is messaging that the display driver ldb has been registered.

Unfortunately I do not get any further - hope you can help. 

Thanks!

------------ 

[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Linux version 4.9.88-gec7d7d8-dirty (root@ubuntu) (gcc version 6.3.1 20170404 (Linaro GCC 6.3-2017.05) ) #5 SMP PREEMPT Sat Jan 2 11:05:59 CET 2021
[    0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] OF: fdt:Machine model: EC-CHARGE powered by Variscite i.MX6 DL/Solo
[    0.000000] debug: ignoring loglevel setting.
[    0.000000] Reserved memory: created CMA memory pool at 0x3c000000, size 320 MiB
[    0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[    0.000000] Memory policy: Data cache writealloc
[    0.000000] On node 0 totalpages: 262144
[    0.000000] free_area_init_node: node 0, pgdat 80f872c0, node_mem_map ab757000
[    0.000000]   Normal zone: 2048 pages used for memmap
[    0.000000]   Normal zone: 0 pages reserved
[    0.000000]   Normal zone: 262144 pages, LIFO batch:31
[    0.000000] percpu: Embedded 14 pages/cpu @ab71b000 s25804 r8192 d23348 u57344
[    0.000000] pcpu-alloc: s25804 r8192 d23348 u57344 alloc=14*4096
[    0.000000] pcpu-alloc: [0] 0 [0] 1 
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 260096
[    0.000000] Kernel command line: console=ttymxc0,115200 ignore_loglevel root=/dev/mmcblk1p2 rootwait rw video=mxcfb0:dev=ldb,LDB-WXGA,if=RGB24,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off
[    0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[    0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[    0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[    0.000000] Memory: 695600K/1048576K available (9216K kernel code, 544K rwdata, 3028K rodata, 1024K init, 457K bss, 25296K reserved, 327680K cma-reserved, 0K highmem)
[    0.000000] Virtual kernel memory layout:
                   vector  : 0xffff0000 - 0xffff1000   (   4 kB)
                   fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
                   vmalloc : 0xc0800000 - 0xff800000   (1008 MB)
                   lowmem  : 0x80000000 - 0xc0000000   (1024 MB)
                   pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)
                   modules : 0x7f000000 - 0x7fe00000   (  14 MB)
                     .text : 0x80008000 - 0x80a00000   (10208 kB)
                     .init : 0x80e00000 - 0x80f00000   (1024 kB)
                     .data : 0x80f00000 - 0x80f883c0   ( 545 kB)
                      .bss : 0x80f8a000 - 0x80ffc7c0   ( 458 kB)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[    0.000000] Preemptible hierarchical RCU implementation.
[    0.000000] Build-time adjustment of leaf fanout to 32.
[    0.000000] RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
[    0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=32, nr_cpu_ids=2
[    0.000000] NR_IRQS:16 nr_irqs:16 16
[    0.000000] L2C-310 erratum 769419 enabled
[    0.000000] L2C-310 enabling early BRESP for Cortex-A9
[    0.000000] L2C-310 full line of zeros enabled for Cortex-A9
[    0.000000] L2C-310 ID prefetch enabled, offset 16 lines
[    0.000000] L2C-310 dynamic clock gating enabled, standby mode enabled
[    0.000000] L2C-310 cache controller enabled, 16 ways, 512 kB
[    0.000000] L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76450001
[    0.000000] Switching to timer-based delay loop, resolution 333ns
[    0.000006] sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns
[    0.000022] clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns
[    0.001323] Console: colour dummy device 80x30
[    0.001339] Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
[    0.001355] pid_max: default: 32768 minimum: 301
[    0.001442] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[    0.001452] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[    0.002051] CPU: Testing write buffer coherency: ok
[    0.002374] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[    0.002439] Setting up static identity map for 0x10100000 - 0x10100058
[    0.169857] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[    0.169966] Brought up 2 CPUs
[    0.169978] SMP: Total of 2 processors activated (12.00 BogoMIPS).
[    0.169984] CPU: All CPU(s) started in SVC mode.
[    0.170780] devtmpfs: initialized
[    0.181596] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[    0.181907] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[    0.181927] futex hash table entries: 512 (order: 3, 32768 bytes)
[    0.200897] pinctrl core: initialized pinctrl subsystem
[    0.201958] NET: Registered protocol family 16
[    0.209185] DMA: preallocated 256 KiB pool for atomic coherent allocations
[    0.239577] cpuidle: using governor menu
[    0.239823] CPU identified as i.MX6DL, silicon rev 1.3
[    0.262145] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[    0.262155] hw-breakpoint: maximum watchpoint size is 4 bytes.
[    0.263232] imx6dl-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
[    0.264922] imx-gpc 20dc000.gpc: Registered imx-gpc
[    0.316861] mxs-dma 110000.dma-apbh: initialized
[    0.320101] SCSI subsystem initialized
[    0.320155] libata version 3.00 loaded.
[    0.320427] usbcore: registered new interface driver usbfs
[    0.320494] usbcore: registered new interface driver hub
[    0.320592] usbcore: registered new device driver usb
[    0.320793] 2000000.aips-bus:usbphy_nop1 supply vcc not found, using dummy regulator
[    0.320925] 2000000.aips-bus:usbphy_nop2 supply vcc not found, using dummy regulator
[    0.322078] i2c i2c-0: IMX I2C adapter registered
[    0.322094] i2c i2c-0: can't use DMA, using PIO instead.
[    0.322957] i2c i2c-1: IMX I2C adapter registered
[    0.322970] i2c i2c-1: can't use DMA, using PIO instead.
[    0.323536] i2c i2c-2: IMX I2C adapter registered
[    0.323549] i2c i2c-2: can't use DMA, using PIO instead.
[    0.323932] Linux video capture interface: v2.00
[    0.323996] pps_core: LinuxPPS API ver. 1 registered
[    0.324003] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.324025] PTP clock support registered
[    0.349634] imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
[    0.351315] imx rpmsg driver is registered.
[    0.351491] Advanced Linux Sound Architecture Driver Initialized.
[    0.352298] Bluetooth: Core ver 2.22
[    0.352350] NET: Registered protocol family 31
[    0.352357] Bluetooth: HCI device and connection manager initialized
[    0.352370] Bluetooth: HCI socket layer initialized
[    0.352382] Bluetooth: L2CAP socket layer initialized
[    0.352415] Bluetooth: SCO socket layer initialized
[    0.353354] clocksource: Switched to clocksource mxc_timer1
[    0.353479] VFS: Disk quotas dquot_6.6.0
[    0.353542] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[    0.364142] NET: Registered protocol family 2
[    0.364732] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[    0.364812] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[    0.364937] TCP: Hash tables configured (established 8192 bind 8192)
[    0.365016] UDP hash table entries: 512 (order: 2, 16384 bytes)
[    0.365054] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[    0.365232] NET: Registered protocol family 1
[    0.365687] RPC: Registered named UNIX socket transport module.
[    0.365695] RPC: Registered udp transport module.
[    0.365699] RPC: Registered tcp transport module.
[    0.365704] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.366416] hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
[    0.367964] Bus freq driver module loaded
[    0.369665] workingset: timestamp_bits=30 max_order=18 bucket_order=0
[    0.376479] NFS: Registering the id_resolver key type
[    0.376504] Key type id_resolver registered
[    0.376509] Key type id_legacy registered
[    0.376554] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[    0.377231] fuse init (API version 7.26)
[    0.383433] io scheduler noop registered
[    0.383442] io scheduler deadline registered
[    0.383633] io scheduler cfq registered (default)
[    0.384214] imx-weim 21b8000.weim: Driver registered.
[    0.386411] mxc_sdc_fb fb@0: registered mxc display driver ldb
[    0.423452] imx-ipuv3 2400000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
[    0.499542] Console: switching to colour frame buffer device 128x48
[    0.537888] imx-sdma 20ec000.sdma: no iram assigned, using external mem
[    0.538461] imx-sdma 20ec000.sdma: loaded firmware 3.3
[    0.543937] pfuze100-regulator 1-0008: unrecognized pfuze chip ID!
[    0.544766] 2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 26, base_baud = 5000000) is a IMX
[    1.170711] console [ttymxc0] enabled
[    1.174052] 21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 72, base_baud = 5000000) is a IMX
[    1.182042] 21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 73, base_baud = 5000000) is a IMX
[    1.189990] 21f0000.serial: ttymxc3 at MMIO 0x21f0000 (irq = 74, base_baud = 5000000) is a IMX
[    1.208542] [drm] Initialized
[    1.210729] [drm] Initialized vivante 1.0.0 20120216 on minor 0
[    1.252964] brd: module loaded
[    1.261607] loop: module loaded
[    1.268745] random: fast init done
[    1.273768] nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xdc
[    1.278823] nand: Micron MT29F4G08ABADAWP
[    1.281536] nand: 512 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64
[    1.287934] gpmi-nand 112000.gpmi-nand: use legacy bch geometry
[    1.292922] gpmi-nand 112000.gpmi-nand: enable the asynchronous EDO mode 5
[    1.298566] Scanning device for bad blocks
[    1.582090] 4 ofpart partitions found on MTD device gpmi-nand
[    1.586563] Creating 4 MTD partitions on "gpmi-nand":
[    1.590321] 0x000000000000-0x000000200000 : "spl"
[    1.595025] 0x000000200000-0x000000400000 : "bootloader"
[    1.600223] 0x000000400000-0x000000c00000 : "kernel"
[    1.605158] 0x000000c00000-0x000040000000 : "rootfs"
[    1.608829] mtd: partition "rootfs" extends beyond the end of device "gpmi-nand" -- size truncated to 0x1f400000
[    1.624987] gpmi-nand 112000.gpmi-nand: driver registered.
[    1.631643] spi_imx 2008000.ecspi: probed
[    1.635199] libphy: Fixed MDIO Bus: probed
[    1.638395] CAN device driver interface
[    1.641155] 2090000.flexcan supply xceiver not found, using dummy regulator
[    1.647764] flexcan 2090000.flexcan: device registered (reg_base=c0a20000, irq=31)
[    1.656192] 2188000.ethernet supply phy not found, using dummy regulator
[    1.773868] pps pps0: new PPS source ptp0
[    1.781539] libphy: fec_enet_mii_bus: probed
[    1.785115] fec 2188000.ethernet eth0: registered PHC device 0
[    1.790125] enc28j60 spi0.0: enc28j60 Ethernet driver 1.02 loaded
[    1.799402] net eth1: enc28j60 driver registered
[    1.802765] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[    1.808053] ehci-mxc: Freescale On-Chip EHCI Host driver
[    1.812289] usbcore: registered new interface driver usb-storage
[    1.817095] usbcore: registered new interface driver usb_ehset_test
[    1.823181] 2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
[    1.833408] ci_hdrc ci_hdrc.0: EHCI Host Controller
[    1.837020] ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
[    1.863396] ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
[    1.868390] hub 1-0:1.0: USB hub found
[    1.870892] hub 1-0:1.0: 1 port detected
[    1.877771] ci_hdrc ci_hdrc.1: EHCI Host Controller
[    1.881379] ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 2
[    1.913409] ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
[    1.918376] hub 2-0:1.0: USB hub found
[    1.920876] hub 2-0:1.0: 1 port detected
[    1.924639] mousedev: PS/2 mouse device common for all mice
[    2.233373] usb 1-1: new high-speed USB device number 2 using ci_hdrc
[    2.433387] rtc-ds1307: probe of 2-0068 failed with error -5
[    2.440835] i2c /dev entries driver
[    2.446441] imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)
[    2.451126] Bluetooth: HCI UART driver ver 2.3
[    2.454353] Bluetooth: HCI UART protocol H4 registered
[    2.458203] Bluetooth: HCI UART protocol LL registered
[    2.462788] sdhci: Secure Digital Host Controller Interface driver
[    2.467703] sdhci: Copyright(c) Pierre Ossman
[    2.470760] sdhci-pltfm: SDHCI platform and OF driver helper
[    2.476105] sdhci-esdhc-imx 2190000.usdhc: could not get ultra high speed state, work on normal mode
[    2.543425] mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA
[    2.555151] sdhci-esdhc-imx 2194000.usdhc: Got CD GPIO
[    2.623536] mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
[    2.633845] mmc0: new DDR MMC card at address 0001
[    2.647947] mmcblk0: mmc0:0001 8GTF4R 7.28 GiB 
[    2.651489] mmcblk0boot0: mmc0:0001 8GTF4R partition 1 4.00 MiB
[    2.659466] mmcblk0boot1: mmc0:0001 8GTF4R partition 2 4.00 MiB
[    2.664427] mmcblk0rpmb: mmc0:0001 8GTF4R partition 3 512 KiB
[    2.672687]  mmcblk0: p1 p2
[    2.703831] mmc1: host does not support reading read-only switch, assuming write-enable
[    2.717434] mmc1: new high speed SDHC card at address aaaa
[    2.722180] mmcblk1: mmc1:aaaa SB16G 14.8 GiB 
[    2.729626]  mmcblk1: p1 p2
[    2.783389] mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
[    2.793387] mxc_vpu 2040000.vpu_fsl: VPU initialized
[    2.797633] mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
[    2.808054] sdhci-esdhc-imx 2198000.usdhc: card claims to support voltages below defined range
[    2.815579] galcore: clk_get vg clock failed, disable vg!
[    2.815777] Galcore version 6.2.4.150331
[    2.858326] mmc2: new high speed SDIO card at address 0001
[    3.256198] caam 2100000.caam: ERA source: CAAMVID.
[    3.259836] caam 2100000.caam: AXI pipeline throttling enabled.
[    3.265663] caam 2100000.caam: device ID = 0x0a16010000000100 (Era 4)
               job rings = 2, qi = 0
[    3.275645] caam_jr 2101000.jr0: Entropy delay = 3200
[    3.340215] caam_jr 2101000.jr0: Instantiated RNG4 SH0.
[    3.400968] caam_jr 2101000.jr0: Instantiated RNG4 SH1.
[    3.411681] caam algorithms registered in /proc/crypto
[    3.419303] caam_jr 2101000.jr0: registering rng-caam
[    3.424111] caam-snvs 20cc000.caam-snvs: can't get snvs clock
[    3.428618] caam-snvs 20cc000.caam-snvs: violation handlers armed - non-secure state
[    3.435475] usbcore: registered new interface driver usbhid
[    3.439752] usbhid: USB HID core driver
[    3.443071] Error: Driver 'mpl3115' is already registered, aborting...
[    3.453174] fsl-ssi-dai 202c000.ssi: No cache defaults, reading back from HW
[    3.463006] NET: Registered protocol family 26
[    3.466882] NET: Registered protocol family 10
[    3.471164] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[    3.476486] NET: Registered protocol family 17
[    3.479648] can: controller area network core (rev 20120528 abi 9)
[    3.484775] NET: Registered protocol family 29
[    3.487934] can: raw protocol (rev 20120528)
[    3.490907] can: broadcast manager protocol (rev 20161123 t)
[    3.495302] can: netlink gateway (rev 20130117) max_hops=1
[    3.499720] Bluetooth: RFCOMM TTY layer initialized
[    3.503312] Bluetooth: RFCOMM socket layer initialized
[    3.507202] Bluetooth: RFCOMM ver 1.11
[    3.509663] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[    3.513700] Bluetooth: BNEP filters: protocol multicast
[    3.517636] Bluetooth: BNEP socket layer initialized
[    3.521301] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[    3.525946] Bluetooth: HIDP socket layer initialized
[    3.529680] 8021q: 802.1Q VLAN Support v1.8
[    3.532603] Key type dns_resolver registered
[    3.537394] cpu cpu0: Registered imx6q-cpufreq
[    3.556245] imx_epdc_fb 20f4000.epdc: can't get/select pinctrl
[    3.571957] imx_thermal 2000000.aips-bus:tempmon: Commercial CPU temperature grade - max:95C critical:90C passive:85C
[    3.582074] hctosys: unable to open rtc device (rtc0)
[    3.586395] tlv320aic3x-supply: disabling
[    3.589112] wlan-en-regulator: disabling
[    3.591736] ALSA device list:
[    3.593465]   No soundcards found.
[    3.606143] EXT4-fs (mmcblk1p2): couldn't mount as ext3 due to feature incompatibilities
[    3.613499] EXT4-fs (mmcblk1p2): couldn't mount as ext2 due to feature incompatibilities
[    3.645520] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)
[    3.652351] VFS: Mounted root (ext4 filesystem) on device 179:34.
[    3.663047] devtmpfs: mounted
[    3.665856] Freeing unused kernel memory: 1024K
[    3.861213] random: crng init done
[    4.136430] systemd[1]: System time before build time, advancing clock.
[    4.192773] ip_tables: (C) 2000-2006 Netfilter Core Team
[    4.215723] cgroup: cgroup2: unknown option "nsdelegate"
[    4.257266] systemd[1]: systemd 241 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRYPTSETUP +GCRYPT +GNUTLS +ACL +XZ +LZ4 +SECCOMP +BLKID +ELFUTILS +KMOD -IDN2 +IDN -PCRE2 default-hierarchy=hybrid)
[    4.278042] systemd[1]: Detected architecture arm.
[    4.316360] systemd[1]: Set hostname to <ec-charge-xxx>.
[    4.609715] systemd[1]: File /lib/systemd/system/systemd-journald.service:12 configures an IP firewall (IPAddressDeny=any), but the local system does not support BPF/cgroup based firewalling.
[    4.625656] systemd[1]: Proceeding WITHOUT firewalling in effect! (This warning is only shown for the first loaded unit using IP firewalling.)
[    5.004004] systemd[1]: Created slice system-getty.slice.
[    5.044435] systemd[1]: Set up automount Arbitrary Executable File Formats File System Automount Point.
[    5.084768] systemd[1]: Listening on udev Kernel Socket.
[    5.152503] systemd[1]: Condition check resulted in Journal Audit Socket being skipped.
[    5.160317] systemd[1]: Listening on initctl Compatibility Named Pipe.
[    6.431367] systemd-journald[218]: Received request to flush runtime journal from PID 1
[    8.781515] usbcore: registered new interface driver usbserial
[    8.795908] usbcore: registered new interface driver usbserial_generic
[    8.801328] usbserial: USB Serial support registered for generic
[    8.847317] usbcore: registered new interface driver option
[    8.851690] usbserial: USB Serial support registered for GSM modem (1-port)
[    8.873850] option 1-1:1.0: GSM modem (1-port) converter detected
[    8.887487] usb 1-1: GSM modem (1-port) converter now attached to ttyUSB0
[    8.905804] option 1-1:1.1: GSM modem (1-port) converter detected
[    8.912412] usb 1-1: GSM modem (1-port) converter now attached to ttyUSB1
[    8.931871] option 1-1:1.2: GSM modem (1-port) converter detected
[    8.953765] usb 1-1: GSM modem (1-port) converter now attached to ttyUSB2
[    8.972071] option 1-1:1.3: GSM modem (1-port) converter detected
[    8.979733] usb 1-1: GSM modem (1-port) converter now attached to ttyUSB3
[   10.071908] wlcore: wl18xx HW: 183x or 180x, PG 2.2 (ROM 0x11)
[   10.080973] wlcore: loaded
[   12.211272] wlcore: PHY firmware version: Rev 8.2.0.0.242
[   12.328366] wlcore: firmware booted (Rev 8.9.0.0.79)
[   12.343302] IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready
[   12.348568] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[   12.455002] Micrel KSZ9031 Gigabit PHY 2188000.ethernet-1:07: attached PHY driver [Micrel KSZ9031 Gigabit PHY] (mii_bus:phy_addr=2188000.ethernet-1:07, irq=-1)
[   12.455129] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[   12.478948] IPv6: ADDRCONF(NETDEV_CHANGE): wlan0: link becomes ready
[   12.598953] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready
[   12.605765] net eth1: link down
[   12.605779] net eth1: normal mode
[   12.606203] net eth1: multicast mode
[   12.606362] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready
[   12.766055] wlcore: down
[   13.286949] wlcore: PHY firmware version: Rev 8.2.0.0.242
[   13.410450] wlcore: firmware booted (Rev 8.9.0.0.79)
[   13.437801] IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready
[   13.447271] wlcore: down
[   13.675140] net eth1: link up - Half duplex
[   13.975330] wlcore: PHY firmware version: Rev 8.2.0.0.242
[   14.069095] wlcore: firmware booted (Rev 8.9.0.0.79)
[   14.093999] IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready
[   14.098976] IPv6: ADDRCONF(NETDEV_CHANGE): eth1: link becomes ready
[   14.104748] net eth1: multicast mode
[   14.182813] net eth1: multicast mode
[   14.187598] net eth1: multicast mode
[   14.242106] net eth1: multicast mode
[   14.333332] net eth1: multicast mode
[   14.335800] net eth1: multicast mode
[   14.341748] net eth1: multicast mode
[   14.568373] IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready
[   16.643943] fec 2188000.ethernet eth0: Link is Up - 1Gbps/Full - flow control off
[   16.650160] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready

 

 

0 项奖励
回复
2 回复数

927 次查看
igorpadykov
NXP Employee
NXP Employee

Hi bit-hauer

 

one can look at example of i.MX6Q with another hdmi bridge (parallel with  sii902x)

 and try to perform similar apprach:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Patch-for-sii902x-hdmi-driver-via-IPU/ta...

 

Best regards
igor

0 项奖励
回复

915 次查看
bit-hauer
Contributor I

Hi Igor,

thanks for your reply, problem has been solved. I went to all configuration again, recognizing that imx-ldb.o is not built - Switching from MXC to IMX video driver system (e.g. CONFIG_IMX_IPUv3_CORE) has solved the issue. Now imx-ldb functions are called and the bridge chip is attached, up and running : ).

Can you perhaps explain the difference between the two "driver systems"?

Thanks so far,

With best regards and Happy New Year!

0 项奖励
回复