How to effect SW2ISO and SW bit in PGC_GPU_PUPSCR register.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to effect SW2ISO and SW bit in PGC_GPU_PUPSCR register.

762件の閲覧回数
t-iishii
Contributor II

Hi all,

In reference manual of i.MX6(IMX6DQRM.pdf) section 27.8.2,

How to work SW2ISO and SW bit in PGC_GPU_PUPSRC and PGC_GPU_PDOWNSRC

on the Wake up sequence Figure 27-5?

Which signal is it triggered the SW2ISO value counter in Figure 27-5 ?

Best regards,

Ishii.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

692件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  The Wake up sequence is as following :

pup_req  ->  (delay of PGC_GPU_PUPSCR[SW]) -> switch_b -> delay of PGC_GPU_PUPSCR[SW2ISO] ->
-> iso

The switch_b signal, triggered with delay of  SW2ISO value counter, is not shown in Figure 27-5.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

692件の閲覧回数
t-iishii
Contributor II

Hello Yuri

Thank you for your response.

I can understand this sequence.

Best regards,

Ishii.

0 件の賞賛
返信