Hi
I find in imx8mm use the QCA9377 and the interface is sdio , but my board is use the QCA6174A which use the pcie. I want to upgrade it to the android 10.10 baseline.
when I insmod the wlan.ko, it shows as below:
[ 4709.296243] wlan: loading driver v4.5.24.4
[ 4709.302185] ath_hif_sdio: HIF (Atheros/multi-bss)
[ 4714.328552] AR6000: Unregistering with the bus driver
How to disable the sdio and change to pcie.
Unfortunately the Wifi Module Driver it is provided by the Module Maker, I think in this case it is a Murata Module, please get in contact with them in order to get a Driver for Android 10. Since in our BSP there is only support for the NXP Wifi chip and the Qualcomm version of SDIO.
I apologize for this inconvenience. But as you understand the driver of the non NXP device should be provide by another maker.