How to disable the sdio wifi and change to pcie wifi

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to disable the sdio wifi and change to pcie wifi

3,347 次查看
94393400
Contributor III

Hi

        I find  in imx8mm use the QCA9377 and the interface is sdio , but my board is use the QCA6174A which use the pcie. I want to upgrade it to the android 10.10 baseline.

when I insmod the wlan.ko, it shows as below:

[ 4709.296243] wlan: loading driver v4.5.24.4
[ 4709.302185] ath_hif_sdio: HIF (Atheros/multi-bss)
[ 4714.328552] AR6000: Unregistering with the bus driver

 

How to disable the sdio and change to pcie.

3 回复数

3,251 次查看
jamesbone
NXP TechSupport
NXP TechSupport

Unfortunately the Wifi Module Driver it is provided by the Module Maker,  I think in this case it is a Murata Module, please get in contact with them in order to get a Driver for Android 10.  Since in our BSP there is only support for the NXP Wifi chip and the Qualcomm version of SDIO.

I apologize for this inconvenience. But as you understand the driver of the non NXP device should be provide by another maker.

0 项奖励
回复

3,251 次查看
94393400
Contributor III

Hi Jamesbone,

        Where to config the SDIO and PCIE, because I use the right wlan.ko, it also show the sdio information.

0 项奖励
回复

3,251 次查看
94393400
Contributor III

Hi,

    In configs files there is a config CONFIG_CLD_HL_SDIO_CORE=y,  needs to change to not set