Hi
I find in imx8mm use the QCA9377 and the interface is sdio , but my board is use the QCA6174A which use the pcie. I want to upgrade it to the android 10.10 baseline.
when I insmod the wlan.ko, it shows as below:
[ 4709.296243] wlan: loading driver v4.5.24.4
[ 4709.302185] ath_hif_sdio: HIF (Atheros/multi-bss)
[ 4714.328552] AR6000: Unregistering with the bus driver
How to disable the sdio and change to pcie.
Unfortunately the Wifi Module Driver it is provided by the Module Maker, I think in this case it is a Murata Module, please get in contact with them in order to get a Driver for Android 10. Since in our BSP there is only support for the NXP Wifi chip and the Qualcomm version of SDIO.
I apologize for this inconvenience. But as you understand the driver of the non NXP device should be provide by another maker.
Hi Jamesbone,
Where to config the SDIO and PCIE, because I use the right wlan.ko, it also show the sdio information.
Hi,
In configs files there is a config CONFIG_CLD_HL_SDIO_CORE=y, needs to change to not set