I have recently modified a qt application to incorporate screen rotation of 90 degrees, However the requirement is now changed to 270 degrees and hence I need to clean my qt recipe before compiling the qt base,
I have tried
bitbake -c clean qt5
but I get an error saying
ERROR: Nothing PROVIDES 'qt5'
this is the path to the bb file I had to modify to compile qtbase
~/yocto_4_9_88_qt/imx-yocto-bsp/sources/meta-qt5/recipes-qt/qt5
the modified file was qtbase_git.bb
this is the link where I got the patch
[meta-qt5] qtbase: Fix the qt5 linuxfb ratation problem - Patchwork
Is there any way I can clean only qtbase?
I don't want to disturb any other recipe.
解決済! 解決策の投稿を見る。
This issue was solved by creating a patch of the changes made and adding it in the path:
~/yocto_4_9_88_q/imx-yocto-bsp/sources/meta-qt5/recipes-qt/qt5/qtbase/
This issue was solved by creating a patch of the changes made and adding it in the path:
~/yocto_4_9_88_q/imx-yocto-bsp/sources/meta-qt5/recipes-qt/qt5/qtbase/
Hello Sujay S,
The error is related to “qt5” not being a valid recipe.
From the patch you shared the changes recipe was “qtbase” so you would need to clean and re-run this recipe instead.
I hope this helps!
Regards,
Hi Gusarambula,
Thank you for the reply,
Should I run bitbake -c clean qtbase and then
build the rootfs using bitbake fsl-image-qt5-validation-imx
or
should I clean entire rootfs using bitbake -c clean fsl-image-qt5-validation-imx
and then build rootfs?