iMX287 can't reset (WDOG is connected to RESETN pin).

cancel
Showing results for 
Search instead for 
Did you mean: 

iMX287 can't reset (WDOG is connected to RESETN pin).

215 Views
eduardo_abian
Contributor I

I have exacly the same problem. How do you fixed it?

0 Kudos
1 Reply

155 Views
Yuri
NXP TechSupport
NXP TechSupport

Hello,

   It is recommended to provide full power OFF -> ON instead of CPU reset, 

since system boot may get hanging because of unpredictable state of external

devices, involved in boot process.  


Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos