How to check whether CDP/DCP is configured

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to check whether CDP/DCP is configured

1,318件の閲覧回数
praneethreddy46
Contributor I

Hi,

Platform : imx6solo/6Dualite based customized board

kernel: 3.10.17

my question is whether charging downstream port (CDP) and Dedicated charging port (DCP) is hardware  or software depenedency ? How can we check whether usb port is  CDP/DCP port ?

Please reply.

Regards,

praneeth

ラベル(2)
0 件の賞賛
返信
1 返信

1,046件の閲覧回数
b36401
NXP Employee
NXP Employee

i.MX6 has hardware USB charger detector block that detects whether the upstream-facing device is connected to a down-stream facing charger, either a dedicated USB charger or a host charger.


Please refer chapter 66.2.7 "Charger detection" of i.MX 6 Processor Reference Manual for the details.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信