How to change the DDR clock frequency

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to change the DDR clock frequency

874 Views
sanketparekh
Contributor II

Hi,

 

I am using H5TC4G63EFR-RDI attached with IMX6DL Processor. With the help of attached XLS file I have configured DDR clock frequency to 400 MHz. How can i configure the DDR clock frequency to below 400 MHz?

 

Thanks and Regards.

Sanket Parekh

Labels (1)
0 Kudos
Reply
1 Reply

861 Views
nxf63675
NXP TechSupport
NXP TechSupport

Hi Sanket,

 

The programming you are using is pretty old, I recommend you to update the version that you are using, on the link bellow you can find the newest version, in this one you can select the DDR clock frequency to bellow 400MHz but please consider the notes that comes on the sheet, this could cause different behaviors than usual.

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX6DQSDL-DDR3-Script-Aid/ta-p/1124443

 

Hope this help you.

Regard,

Israel H.

 

0 Kudos
Reply