Using an imx8mm I need to boot the M4 as quickly as possible. Using u-boot scripting with a 0 autoboot abort delay gets me below 3 seconds but we need to get faster than that.
The plan is to open up u-boot to load and run the M4 immediately before the autoboot abort delay. Does anyone have any advice on going down this path?
TIA
If the M4 is brought out of reset before u-boot runs can it execute from SPI Flash? If so, is it possible to program the SCU to start the M4? I haven't drilled down in the SCU code yet.
The u-boot script doesn't run until after the autoboot abort option delay expires. Using this method takes 2+ seconds to get to the abort prompt plus any delay at the prompt before the command can start running. I need to boot the M4 before the prompt.
I am afraid there is no easy way to boot M4 core early without changing u-boot logic.
However we have no suggestions to add booting M4 core in the very beginning of u-boot.
Sorry for the inconvenience.