Hi community.
I am currently using an i.MX6 SabreAI board.
I want to boot linux directly from serial downloader mode without writing to emmc or QSPI or SD card.
Is such usage possible?
I have already checked the following documents, but I do not understand the procedure.
whether it can be used in such a way
If possible, could you please tell me the command procedure?
UUU (Universal Update Utility)Document (uuu.pdf)
https://github.com/nxp-imx/mfgtools
LF5.15.71.2.2.0のLinuxUserGuide
已解决! 转到解答。
i.mx6 can boot up from usb, you can refer to the old community link