Hi community.
I am currently using an i.MX6 SabreAI board.
I want to boot linux directly from serial downloader mode without writing to emmc or QSPI or SD card.
Is such usage possible?
I have already checked the following documents, but I do not understand the procedure.
whether it can be used in such a way
If possible, could you please tell me the command procedure?
UUU (Universal Update Utility)Document (uuu.pdf)
https://github.com/nxp-imx/mfgtools
LF5.15.71.2.2.0のLinuxUserGuide
解決済! 解決策の投稿を見る。
i.mx6 can boot up from usb, you can refer to the old community link
i.mx6 can boot up from usb, you can refer to the old community link
thank you for your reply. I will check the docs and give it a try.