How do I run qt app on IMX8?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I run qt app on IMX8?

2,335件の閲覧回数
kangmw086
Contributor III

i used imx8mq-evk.

I ran the qt app on the evk board.
However, you can not connect to ssh root and run qt app in the same way.
And is it possible to overlay qt and camera on IMX8MQ-EVK?
I need an example.
YOCTO BUILD INFO
https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-rocko -m imx-4.9.88-2.0.0_ga.xml
DISTRO=fsl-imx-wayland MACHINE=imx8mqevk source fsl-setup-release.sh -b build-wayland
regards.
0 件の賞賛
2 返答(返信)

1,731件の閲覧回数
art
NXP Employee
NXP Employee

Please refer to the Section 8 "Graphics" of the attached document.

0 件の賞賛

1,731件の閲覧回数
kangmw086
Contributor III

Is it possible only for FB, XWAYLAND, X11?

I wonder if it is possible in WAYLAND.

0 件の賞賛