How do I run qt app on IMX8?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I run qt app on IMX8?

2,334 Views
kangmw086
Contributor III

i used imx8mq-evk.

I ran the qt app on the evk board.
However, you can not connect to ssh root and run qt app in the same way.
And is it possible to overlay qt and camera on IMX8MQ-EVK?
I need an example.
YOCTO BUILD INFO
https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-rocko -m imx-4.9.88-2.0.0_ga.xml
DISTRO=fsl-imx-wayland MACHINE=imx8mqevk source fsl-setup-release.sh -b build-wayland
regards.
0 Kudos
2 Replies

1,730 Views
art
NXP Employee
NXP Employee

Please refer to the Section 8 "Graphics" of the attached document.

0 Kudos

1,730 Views
kangmw086
Contributor III

Is it possible only for FB, XWAYLAND, X11?

I wonder if it is possible in WAYLAND.

0 Kudos