How do I run qt app on IMX8?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How do I run qt app on IMX8?

2,365 次查看
kangmw086
Contributor III

i used imx8mq-evk.

I ran the qt app on the evk board.
However, you can not connect to ssh root and run qt app in the same way.
And is it possible to overlay qt and camera on IMX8MQ-EVK?
I need an example.
YOCTO BUILD INFO
https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-rocko -m imx-4.9.88-2.0.0_ga.xml
DISTRO=fsl-imx-wayland MACHINE=imx8mqevk source fsl-setup-release.sh -b build-wayland
regards.
0 项奖励
2 回复数

1,761 次查看
art
NXP Employee
NXP Employee

Please refer to the Section 8 "Graphics" of the attached document.

0 项奖励

1,761 次查看
kangmw086
Contributor III

Is it possible only for FB, XWAYLAND, X11?

I wonder if it is possible in WAYLAND.

0 项奖励