Dear:
Currently I am working on IMX8QM-MEK board running with Android Automotive 11.0.0_1.1.0 (Linux 5.4.47 Kernel).
After I connect IMX-AUD-IO board FR FL, using AUDIO SLOT 1. I tried play audio through cs42888:
$tinyplay xx.wav -D 1
but it did not work ,In the system, i can find card0:bt-sco , card1:cs42888,card2:wm8960.
does the system default music output from the AUD board through CS42888?
and i find something from references:
but In the source code, I can't find Similar fields cs42888_bus_name or wm8960_card.bus_name.
How can i hear anything from IMX-AUDIO-IO board with IMX8QM
解決済! 解決策の投稿を見る。
Solved. I forgot shorting the pins 2&3...
Hi,
Could you help me with this issue?
I am also not getting audio through these ports.
However, in your solution you say you solved using shorting PIN2 & 3. Could you kindly elaborate?
If so, could you let me know from where you get this info?
Below is the error, I am getting.
10-28 07:53:30.318 367 2263 I audio_hw_primary: start_output_stream: primary: 1, out: 0xf36437c0, device: 16777216, address: bus0_media_out, mode: 0, flags 0x2
10-28 07:53:30.318 1908 1908 I MediaServiceManager: >onPlaybackStarted: 1
10-28 07:53:30.318 367 2263 I audio_hw_primary: select_output_device(), headphone 0 ,headset 0 ,speaker 2
10-28 07:53:30.318 367 2263 E audio_hw_primary: Failed to find card from bus 'bus0_media_out'
10-28 07:53:30.318 367 2263 D audio_hw_primary: start_output_stream: pcm_open: card: -1, pcm_device_id: 0, rate: 48000, channel: 2, format: 0, period_size: 0xc0, flag: 9
10-28 07:53:30.318 367 2263 E audio_hw_primary: start_output_stream: Invalid PCM card id: -1
10-28 07:53:30.319 367 1123 I audio_hw_primary: start_output_stream: primary: 0, out: 0xf3642b60, device: 16777216, address: bus1_system_sound_out, mode: 0, flags 0x2
10-28 07:53:30.319 367 1123 I audio_hw_primary: select_output_device(), headphone 0 ,headset 0 ,speaker 2
10-28 07:53:30.319 367 1123 D audio_hw_primary: start_output_stream: pcm_open: card: 1, pcm_device_id: 0, rate: 48000, channel: 2, format: 0, period_size: 0xc0, flag: 9
i just shorted pins 2 and 3 , the J47 on the base board
Hi,
May I know how you got this information. Is it recorded in any technical documents of NXP?
Thank you.
mek_8q:/data/user # tinymix -D 1
Mixer name: 'cs42888-audio'
Number of controls: 22
ctl type num name value
0 INT 2 DAC1 Playback Volume 255 255
1 INT 2 DAC2 Playback Volume 255 255
2 INT 2 DAC3 Playback Volume 255 255
3 INT 2 DAC4 Playback Volume 255 255
4 INT 2 ADC1 Capture Volume 230 230
5 INT 2 ADC2 Capture Volume 230 230
6 BOOL 2 DAC1 Invert Switch Off Off
7 BOOL 2 DAC2 Invert Switch Off Off
8 BOOL 2 DAC3 Invert Switch Off Off
9 BOOL 2 DAC4 Invert Switch Off Off
10 BOOL 2 ADC1 Invert Switch On On
11 BOOL 2 ADC2 Invert Switch On On
12 BOOL 1 ADC High-Pass Filter Switch On
13 BOOL 1 DAC De-emphasis Switch Off
14 ENUM 1 ADC1 Single Ended Mode Switch Differential
15 ENUM 1 ADC2 Single Ended Mode Switch Differential
16 INT 1 DAC Single Volume Control Switch 1
17 ENUM 1 DAC Soft Ramp & Zero Cross Control Switch Immediate Change
18 BOOL 1 DAC Auto Mute Switch On
19 BOOL 1 Mute ADC Serial Port Switch Off
20 INT 1 ADC Single Volume Control Switch 1
21 ENUM 1 ADC Soft Ramp & Zero Cross Control Switch Immediate Change
should I change any value by tinymix?
Hi Zilun
one can try to check if it works in linux, use imx8qm-mek.dts
sect.7.5 Audio Mixer (AUDMIX) i.MX Linux Reference Manual
https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_amix_test?h=imx_5.4.47_2.2.0
Best regards
igor