In im8m evb board & Linux image.Seem the GPU frequency is fixed at 800 MHz.
But I check the GPU frequency can be boom up to 1000 MHz.
If don't consider overheat problem, how can I set to 1000 MHz?
Thanks.
Hi Liou
one can look on
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov,
Thanks for replay!
There are some questions:
1. Only set IMX8MQ_CLK_GPU_SHADER_SRC to 1000 MHz?
Is IMX8MQ_CLK_GPU_CORE_SRC, IMX8MQ_CLK_GPU_AXI_SRC, and IMX8MQ_CLK_GPU_AHB_SRC don't set to 1000 MHz?
2. The imx8mq datasheet say the gpu clcok if gets to 1G Hz, need 1V voltage
Will it auto adjust voltage to 1V, or need to do some setting manually?