One of the best sources of information and example source code for using the V4L2 interface in the Linux BSP are the unit tests provided by Freescale. This code provides a concise example of how to accomplish basic functionalities which can be used a building blocks for your more complex use cases. The unit test source code can be accessed using the following ltib command:
./ltib -m prep -p imx-test
Afterward, the source code will be located in your ltib project directory in the following location:
<ltib install dir>/rpm/BUILD/imx-test-<version>/
This source code contains a wealth of information that hopefully will help you shorten the time it takes to get up and running with these sometimes complicated APIs.
解決済! 解決策の投稿を見る。
Yes. Getting the source is the same process as before. Using LTIB perform the following: ./ltib -m prep imx-test . This will unpack the sources in the rpm/BUILD/ directory of your LTIB project.
For the fb test, you just need to have the framebuffer driver in the system. For ipudev, libipu is necessary.
GStreamer does not require X Windows. You can directly use the ipulib sink or the v4l2 sink plug-in for rendering video in a non-X environment.
Does Freescale provide the source code for imx-test anymore? I finally found it here. Is there an official version?
Yes. Getting the source is the same process as before. Using LTIB perform the following: ./ltib -m prep imx-test . This will unpack the sources in the rpm/BUILD/ directory of your LTIB project.
I couldn't find the source code for the unit tests anywhere in any package, is it in imx-test-11.09.01-1.arm.rpm?
$ ./ltib -m prep imx-test
The options prep, scbuild, scinstall and scdeploy are only allowed when working
on a single package, not a list. You need to supply the option -p|--pkg <pkg>
$ ./ltib -p imx-test
Processing platform: Freescale iMX5x Based Boards
===================================================
using config/platform/imx/.config
Processing: imx-test
======================
Started: Tue Oct 16 23:23:24 2012
Ended: Tue Oct 16 23:23:27 2012
Elapsed: 3 seconds
Build Succeeded
lucid@ubuntu:~/Desktop/B/ltib$ find . |grep imx-test
./rpm/BUILD/linux-2.6.35.3/patches/0247-ENGR00131944-Fix-imx-test-build-failure-issue-on-mx2.patch
./rpm/RPMS/arm/imx-test-11.09.01-1.arm.rpm
./dist/lfs-5.1/mxc-misc/imx-test.spec
Sorry about that. There is a command line option missing: ./ltib -m prep -p imx-test
Thanks, that works. I hadn't seen any documentation for that
Thank you, indeed these might be useful building blocks.
What are the prerequisites for the graphics related test tools?
imx-test-11.09.01/test/mxc_fb_test/
imx-test-11.09.01/test/mxc_ipudev_test/
I am building the software from scratch, not running the supplied image, and would like to learn what I need to bring up in order to run these tests.
Same question for the Freescale supplied GStreamer components; do these require the X Windows to be up and running on the target?